PCIe: Virtual channels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe: Virtual channels

6,927件の閲覧回数
julian_dietrich
Contributor I

Hey all,

I need to know which NXP MCUs/MPUs supports more then one Virtual Channel (VC) for PCIe.

I need to realize isochronous data transfers over PCIe.

Thanks in advance!

0 件の賞賛
返信
5 返答(返信)

6,248件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Julian

virtual channels are supported, for example this is described in

sect.48.2.4 Configuration-Dependent Module (CDM)

i.MX 6Dual/6Quad Applications Processor Reference Manual

or sect.19.2.1.2 Features

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,248件の閲覧回数
julian_dietrich
Contributor I

Thanks Igor!

Maybe I'm blind but in both documents I can't find any answer about how many VC's are supported?

Furthermore I'm quite new in the PCIe-technology and I have a general question:

I want to connect several PCIe-endpoints via a PCIe-switch and the communication between the endpoints must be isochronous.

Is it true, that for isochronous data transfers I need more then one VC also in the endpoints?

Or are the several VCs only for the PCIe switch required?

0 件の賞賛
返信

6,248件の閲覧回数
dav1
Contributor V

[email protected] Did you solve this? curious which pcie switch you used?

0 件の賞賛
返信

6,248件の閲覧回数
julian_dietrich
Contributor I

Hi dav1,

It turns out that you need the VC-capability for all connected PCIe-parts in the system. So while the enumeration phase, the RC will scan the capabilities of each part/port, and when the Endpoint has only one VC, the hole communication path between RC/Switch/EP will only use one VC, even if the switch itself has more than one VC.

For me it doesn't make sense - but that's the way it works...

In the end we kicked all VC/TC-schemes for our system. It is very less supported by manufactures, especially for EPs.

We're going the way to only have realtime/isochronous data in our system. Thus, we won't have to seperate these data streams via VC/TC anymore.

0 件の賞賛
返信

6,248件の閲覧回数
dav1
Contributor V

Thanks for the comments Julian,

what switch IC did you use?

0 件の賞賛
返信