PCIE_CTRL0_WAKE_B level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCIE_CTRL0_WAKE_B level

3,012 次查看
mohamed-ali_fod
Contributor I

Hello,

I have the same issue as https://community.nxp.com/t5/i-MX-Processors/i-MX8-QuadXPlus-GPIO-configuration/td-p/1404411

Could you provide details why the PCIE_CTRL0_WAKE_B is always high on i.MX8 QuadXPlus MEK, I checked that there is a pull up resistor, can this signal be low?

Could you please also let me know how to enable wakeup on that PCIE pin coming from wifi module? I am using linux-imx-6.1

Best regards,

Mohamed Ali

0 项奖励
回复
4 回复数

2,922 次查看
mohamed-ali_fod
Contributor I

Hi @riteshmpatel,

Thank you but in evk it seems that the wifi module doesn't use PCIE_CTRL0_WAKE_B for wakeup? Shall I configure PCIE_CTRL0_WAKE_B from SCFW as wakeup event coming from PCIe wifi module? Where I can find an example code?

Best regards,

Mohamed Ali

0 项奖励
回复

2,908 次查看
gnar_fang
NXP Employee
NXP Employee

PCIE_CTRL0_WAKE_B as input pin we can't control it.

some details I will check it and reply to you later.

0 项奖励
回复

2,890 次查看
gnar_fang
NXP Employee
NXP Employee

@mohamed-ali_fod  

Do you mean to use the wifi to wake up the Host system?

0 项奖励
回复

2,937 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @mohamed-ali_fod,

I hope you are doing well.
Please accept my apologies for the delay in response.

PCIE_CTRL0_WAKE_B because it's input Pin. PCIE EP pulls it down.
One can refer to wifi_wake_host in imx8mp-evk.dts

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复