i.MX8 QuadXPlus GPIO configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 QuadXPlus GPIO configuration

662 Views
nagarajan-r
Contributor I

Hi,

I have been using i.MX8 QuadXPlus MEK Evaluation board running on QNX 7.1 RTOS.

I am able to boot the board in QNX 7.1 with the BSP provided the qnx for this board.

the below code is part of the Startup program present in QNX 7.1 BSP.

imx_pad_t pads[] = {

{SC_P_PCIE_CTRL0_WAKE_B, IMX_PAD_ALT_4, SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF, SC_PAD_28FDSOI_DSE_DV_LOW, SC_PAD_28FDSOI_PS_NONE}, }

set_28fdsoi_pad(startup_data->ipc, &pads[0], sizeof(pads) / sizeof(imx_pad_t));

the above function calls the below 2 functions.

sc_pad_set_mux(ipc, pads[i].pad, pads[i].mux, pads[i].cfg, pads[i].iso);

sc_pad_set_gp_28fdsoi(ipc, pads[i].pad, pads[i].dse, pads[i].ps);

once the mux configuration is done, i am calling the application code 

out32(gpio4_base + IMX_GPIO_GDIR, (in32(gpio4_base + IMX_GPIO_GDIR) & ~(0x01 << 2)));

if((0x01 << 2) & in32(gpio4_base + IMX_GPIO_DR))
{
printf("PCIE_CTRL0_WAKE_B is set\n");
}
else
{
printf("PCIE_CTRL0_WAKE_B is not set\n");
}

observation: even though this GPIO pin is pulled high by default, this code always reads low. I am unable to figure out what is the issue. Any support on this is really appreciated.

Thanks

Nagaraj

0 Kudos
Reply
1 Reply

642 Views
Yuri
NXP Employee
NXP Employee

@nagarajan-r 
Hello,

   I've sent some comments directly.

Regards,
Yuri.

0 Kudos
Reply