PCIE CLOCK GENERATOR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCIE CLOCK GENERATOR

2,528 次查看
HM_BDBA
Contributor I

Hello NXP Team

 

I have a query regarding PCIe clock generator used in 8MPLUS-BB Reference Board . 

As per reference board to use internal clock, (When using internal clock populate R135, R136, remove R131, R132, R137, R138) , Have NXP validated reference board with internal clock (clock sources by iMX 8M plus processor to peripheral, without using pcie clock generator) , Is that solution working ?

Do Pcie Clock Generator necessary for iMX 8M plus  ?

 

HM_BDBA_0-1651052625240.png

 

0 项奖励
回复
2 回复数

2,491 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

On EVK, a PCIE clock generator chip (9FGV0241) is used to feed high-quality clock to both the PHY and connecter/device. If a PCIE clock generator is not available, use the internal clock of the chip. Note that the internal clock exhibits larger jitter than that from PCIE clock generator.

0 项奖励
回复

2,512 次查看
HM_BDBA
Contributor I

Hello NXP 

 

Please respond on this query. 

0 项奖励
回复