PCI interface in imx6 saberauto board not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCI interface in imx6 saberauto board not working

2,111 Views
ashutosh10509
Contributor I

I am trying to connect Atheros Wifi chip to PCI-E interface of imx6 saberauto board but it's is not working.

After analyzing the boot logs ,  i found that PCI-E link is down.

I am not able to figure it out why i am PCI-E link down error.

Attached is the boot logs.

 

I have already enabled all  the drivers required for PCI-E interface using LTIB.

Original Attachment has been moved to: imx6_board.log.zip

0 Kudos
Reply
3 Replies

1,821 Views
hanseunglee
Contributor III

Did you solve the PCI issue ? I also have a same problem.

In my case, to do below.

1. ltib$./ltib -m config

     - check Always rebuild the kernel

     - check Configure the kernel

     save and exit

2.  ltib$./ltib

     .config - Linux kernel Configuration

     -  System Type enter

          - Freescale MXC Implementations enter

               - chkeck PCI Express support

     - Bus support enter

          - check Message Signaled Interrupts(MSI and MSI- X)

          - check PCI Express support

     - Networking support enter

          - wireless enter

               - check Generic IEEE 802.11 Networking Stack(mac80211)

     - Device Drivers

          - check Network device support

               - Wireless LAN enter

                    - check Atheros Wireless Cards

                         -  Atheros 802.11n wireless cards support (just my case)

save end exit

That is  all when I ready for PCIe wifi card install. But I could not success install driver(can not run on imx6q -sabresd board)

If you have a solution, please tell me.

0 Kudos
Reply

1,821 Views
igorpadykov
NXP Employee
NXP Employee

Hi ashutosh

according to log, TO1.1 preproduction chip is used.

It is not supported in BSPs, refer to attached Release Notes

Table 7. Known Issues.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,821 Views
ivannikolaenko
Contributor IV

Hi

Did you solve the PCI issue? I can't get i.MX6q PCI working too.

0 Kudos
Reply