Overrun while recording audio file into SD card using Imx35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overrun while recording audio file into SD card using Imx35

1,353 Views
mailbriandavid
Contributor I

Hi,

   I need to record/write files(maybe large upto 1 gb) into a SD card without any overrun or missing in minimum constant speed of 16 MB/sec.  Is that  possible with using I.MX 35 processor and a class 10 SD card of "sandisk Extreme"? With my I.MX 35 processor, I got overrun.   What all possible ways which i can record audio into SD card with  a minimum constant speed of 16 MB/sec?

Regards,

Brian

Labels (1)
2 Replies

1,169 Views
LeonardoSandova
Specialist I

I am not familiar with imx35, but you can try placing the bootloader on a location which is not the SD card, then indicating the kernel to mount the filesystem on it. If this works, you may have the speed you required.

Leo

0 Kudos
Reply

1,169 Views
Yuri
NXP Employee
NXP Employee

I have some doubts regarding 16 MBytes/sec for SD cards (even of class 10).

To test maximum real write performance, please try the next Linux commands (as an example) :

# mount /dev/mmcblk0p1 /mnt/cdrom

# time nice -n -10 dd if=/dev/zero of=/mnt/cdrom/file.tst bs=1M count=1000