Output format of imx vpu decoder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output format of imx vpu decoder

Jump to solution
1,926 Views
girijapretha
Contributor II

Hi,

I am using decode-example from libimxvpuapi package to decode h264 file.

I am not sure about the output format of the decoder. Is it YUV420 or YUV422?

If it is not YUV422, can we decode h264 file to produce YUV422(YUYV) output?

Thanks in advance

Labels (4)
0 Kudos
Reply
1 Solution
1,730 Views
joanxie
NXP TechSupport
NXP TechSupport

1) vpu output is yuv420

2) yes, you can decode h264 in yuv422

View solution in original post

2 Replies
1,731 Views
joanxie
NXP TechSupport
NXP TechSupport

1) vpu output is yuv420

2) yes, you can decode h264 in yuv422

1,730 Views
shivaeruventi
Contributor III

Can VPU produce RGB out format instead of YUV formats?

0 Kudos
Reply