Ota zip File isgetting updated with boot.img,bootloader.imgThu, Jul 14 2011 23:58:32 and META_INFO with may 19 2017 with in imx6dq on andriod MARSHMELLOW

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ota zip File isgetting updated with boot.img,bootloader.imgThu, Jul 14 2011 23:58:32 and META_INFO with may 19 2017 with in imx6dq on andriod MARSHMELLOW

1,981 次查看
ayyappadasps
Contributor II

i am following the below steps

please help me???????????

OTA update

1. TO build the source we are using the script file ->android_build.sh

2. To build the ota package i am following the below commands


source build/envsetup.sh
lunch sabresd_6dq-user
make

3.After the make success i am doing the following for getting ota file


make otapackage

make PRODUCT=sabresd_6dq-user otapackage -j4

then obtainment is below

-rw-rw-r-- 1 zumi-02 zumi-02 8865064 Jul 14 2011 boot.img
-rw-rw-r-- 1 zumi-02 zumi-02 445440 Jul 14 2011 bootloader.img
-rw-rw-r-- 1 zumi-02 zumi-02 15407 Jul 14 2011 file_contexts
drwxrwxr-x 3 zumi-02 zumi-02 4096 May 19 19:18 META-INF
-rw-rw-r-- 1 zumi-02 zumi-02 536698880 Jul 14 2011 system.new.dat
-rw-rw-r-- 1 zumi-02 zumi-02 0 Jul 14 2011 system.patch.dat
-rw-rw-r-- 1 zumi-02 zumi-02 345 Jul 14 2011 system.transfer.list

标签 (4)
0 项奖励
回复
2 回复数

1,728 次查看
ayyappadasps
Contributor II

Hi jimmychan

                        i followed the same procedure in question 30 .but i am not getting any updated zip file

0 项奖励
回复

1,727 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Attached is the FAQ for Android BSP. you can find the OTA information in section 30.

0 项奖励
回复