OrCAD Symbol file for iMX6 Dual Processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OrCAD Symbol file for iMX6 Dual Processor?

ソリューションへジャンプ
2,370件の閲覧回数
thilakrao
Contributor I

Hi,

Can anyone share the link from where I can download the OrCAD Symbol file for iMX6 Dual Processor. I got an OrCAD Library file for iMX6 DualLite from this forum. Can I use the same?

And also please let me know, where can I find the details about the PIN variations in different iMX6 variants?

Thank you.

Regards,

Thilak

ラベル(1)
1 解決策
2,172件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Thilak,

You can go to our website to download the rCAD Symbol file for iMX6 Dual Processor. The i.mx6DUAL is not the same as iMX6 DualLite. The i.MX6 Dual is completely compatible with i.MX6Q, the hardware design is the same and also BSP is the same. The difference is that the i.MX6Q CPU has 4 cores and the  i.MX6 Dual only has 2. The rCAD Symbol file for iMX6 Dual Processor you can download by this link Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emu... . You can see i.MX 6Dual Processors|Advanced 3D Graphics|NXP under the Printed Circuit Boards and Schematics - Schematics (4).

About the pin variations you can refer to our datasheet and reference manual document. Also you can use our IOUMUX TOOL, it will do help to you.
Have a nice day
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,173件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Thilak,

You can go to our website to download the rCAD Symbol file for iMX6 Dual Processor. The i.mx6DUAL is not the same as iMX6 DualLite. The i.MX6 Dual is completely compatible with i.MX6Q, the hardware design is the same and also BSP is the same. The difference is that the i.MX6Q CPU has 4 cores and the  i.MX6 Dual only has 2. The rCAD Symbol file for iMX6 Dual Processor you can download by this link Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emu... . You can see i.MX 6Dual Processors|Advanced 3D Graphics|NXP under the Printed Circuit Boards and Schematics - Schematics (4).

About the pin variations you can refer to our datasheet and reference manual document. Also you can use our IOUMUX TOOL, it will do help to you.
Have a nice day
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,172件の閲覧回数
thilakrao
Contributor I

Thank you Dan.

I have downloaded from the links you provided. I understand "SABRESDB_DESIGNFILES" are the exact reference file for iMX6 Dual Processor.

I just wanted to know whether the rCAD symbol file for iMX6D is explicitly available in the site. Because I was not able to find it. What I have done it is that I have copied the iMX6 symbol from the design cache of the "SPF-27516_C5.DSN" schematic.

Are there any link where only the library file for iMX6D is available? ..

Whatever you have provided now doesn't have the libraries explicitly so I have copied it from the schematic file. Is that fine?

Please let me know.

Thank you.

Regards,

Thilak

0 件の賞賛
返信
2,172件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Thilak,

The i.MX6 Dual is completely compatible with i.MX6Q. So about the i.MX6D design you can refer to the i.MX6Q.

Have a nice day

Dan