Hi all,
I'm working on integrating ZTE 3G modem on the imx6 processor running Android 4.4. The ZTE modem is integrated and I'm using the ZTE provided libreference-ril.so library.
While booting the device, the rild and rild-debug sockets are getting created and a set of AT commands works and suddenly the rild daemon is exiting and it is trying to restart the daemon continuously, thereby making my complete Telephony operations to halt.
Attached is the log for the same.
Any pointers for debugging the issue would be very much helpful.
Regards
Original Attachment has been moved to: putty.log.zip
its the library error. Got the source and recompiled it locally.
Could you share the source? I am testing the zte 3g function, but can not find the related libreference-ril.so