Optimized v4l2src gstreamer plugin for I.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Optimized v4l2src gstreamer plugin for I.MX8

3,524 Views
nissim_beja
Contributor I

Dear All,

Is there an optimized v4l2src gstreamer plugin, that utilizes the I.MX8 hardware blocks like DMA component (to reduce video pipeline latency) for the I.MX8 processors?  if not, is there any plan to provide such in the future? 

I found that there is such plugin for the I.MX6 (imxv4l2video).

 

Thanks,

Nissim.

0 Kudos
Reply
3 Replies

3,349 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nissim

MX8 specific plugins are listed in Table 15. i.MX GStreamer 1.0 plugins

attached Release Notes. Example with v4l2src :

gst-launch-1.0 v4l2src ! video/x-raw,width=640,height=480 ! \
v4l2h264enc extra-controls="controls,h264_entropy_mode=0,video_bitrate=245000;" ! \
h264parse ! v4l2h264dec ! queue ! waylandsink sync=false

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,350 Views
nissim_beja
Contributor I

Hi Igor,

Does it mean that the I.MX8 uses the standard v4l2src plugin? 

if its true are there plans to provide such plugin that utilizes the hardware of the I.MX8 Processor (like in I.MX6)?

0 Kudos
Reply

3,350 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nissim

 

no such plans, sorry.

 

Best regards
igor

0 Kudos
Reply