Operating Ranges for VDD_SOC_IN when it operate over 328MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Operating Ranges for VDD_SOC_IN when it operate over 328MHz

1,571件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

 

Could you tell me the operating range for VDD_SOC_IN when it operate over 328MHz ?

 

Ko-hey

 

ラベル(3)
0 件の賞賛
返信
1 返信

1,501件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

for i.MX6DL VPU operation > 328MHz is not specified, according

to Table 69-2. VPU Clocks i.MX6SDL Reference Manual :

"VPU functional clock. Controls all VPU decoding functionality, with a
maximum frequency of 328 MHz."

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信