OpenSSL, using CAAM, signature verification fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenSSL, using CAAM, signature verification fail

1,727 Views
noammoshe
Contributor II

When using the CAAM (Cryptographic Accelerator and Assurance Module) module in IMX6 via OpenSSL I'm getting a 'Segmentation fault' due to 'Cannot allocate memory'. strace:

pastedImage_1.png

I'm trying to verify a signature of a large file (~700MB).

OpenSSL default engine ('Dynamic engine loading support'), software implementation, is working fine. When using '(cryptodev) BSD cryptodev engine' engine (with CAAM) the file verification fail.

Is anyone can assist? is it a known issue of CAAM?   

Info about the connection of CAAM to OpenSSL:

https://www.digi.com/resources/documentation/digidocs/90001546/reference/android/r_caam_android.htm
http://trac.gateworks.com/wiki/ventana/encryption

Tags (3)
0 Kudos
Reply
1 Reply

1,354 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please check memory (over night mode), using the Stress test :

i.MX6/7 DDR Stress Test Tool V2.70 

  Try the recent NXP BSPs. Please look at section 9 (Security) of "i.MX_Linux_User's_Guide.pdf"

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.0.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply