OpenGL issue with QT5 qml applications on I.MX53-based board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenGL issue with QT5 qml applications on I.MX53-based board

2,507 Views
alexanderdyakon
Contributor I

Hi everyone.


First of all, sorry for my English)

I have DIGI ConnectCore development kit, based on I.MX53 microprocessor, on which iI'm trying to launch QT5 QML-based application. But building rootfs image by means of Yocto does not bring good result.

I use Ubuntu (64-bit version 14.04) virtual machine and following meta-layers (both "daisy" and "dizzy" branches I've tried):

  1. those one from Freescale community (fsl-community-bsp, https://github.com/Freescale/fsl-community-bsp-platform);
  2. meta-qt5 layer (https://github.com/meta-qt5/meta-qt5)

I have already tried fsl-image-multimedia(-full) recipe with modified local.conf, which contents concering QT5 I get from this link: http://wiki.wandboard.org/index.php/Building_Qt5_using_yocto_on_Wandboard.

I have to say, builds was successfull, but I haven't managed to launch QT Quick based applications (those one based on widgets runs well), and I've got following errors from debug console, when I run app under X-window system (by using "-platform xcb" postfix):

Could not find of the system's Compose files. Consider setting the QTCOMPOSE environment setting.

QxbIntegration: cannot create platform opengl context, neither GLX nor EGL enabled

Failed to create openGL context for format qsurfaceformat

and such errors I've got when run with eglfs plugin (-platform eglfs):

Could not find of the system's Compose files. Consider setting the QTCOMPOSE environment setting.

Could not create the egl surface: error = 0x300b.

I realize that such messages points to OpenGL-related problems, but I cannot understand, what's the reason. GPU-related packages are included in build (I mean "amd-gpu-bin-mx51" and "imx-vpu"). I have tried both X and direct framebuffer (by adding DISTRO_FEATURES_remove = "x11 wayland" in local.conf ) variants, but with no success.

Do I need to get some special packages on configs in order to get QML applications working? May be there is more proper way?

Tags (4)
0 Kudos
Reply
1 Reply

1,195 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

Have not try on MX53 qith Ubuntu 14.04 as host but This solution works for me, i strongly recommend to take a look:

Qt Imx53 gstreamer

Regards

0 Kudos
Reply