OpenGL MM06 & MM07 Benchmark

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenGL MM06 & MM07 Benchmark

ソリューションへジャンプ
2,368件の閲覧回数
wei-fonglin
Contributor II

Hi All,

We would like to run test cases 3.6.1 and 3.6.2 in AN4509.pdf.

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf

But we don't know where to download the MM06 and MM07.

Can Freescale provide these two benchmark application or where should we buy/download these ?

Many Thanks

Frank

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
2,074件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Frank,

     The software is designed by Futuremark :http://cn.futuremark.com/benchmarks/3dmark

      you can contact them and buy it !

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,075件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Frank,

     The software is designed by Futuremark :http://cn.futuremark.com/benchmarks/3dmark

      you can contact them and buy it !

Regards,

Weidong

0 件の賞賛
返信