OpenGL ES with fbdev

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenGL ES with fbdev

4,263 Views
BrianEdmond
Contributor II

I am trying to get OpenGL ES running with fbdev and not X11 however I can't seem to even run the tutorials.  eglInitialize fails on the board and I also have to link against the X libs for EGL.  Has anyone gotten the OpenGL ES tutorials running without X11?

 

Thanks,

Brian

Labels (1)
0 Kudos
Reply
4 Replies

3,077 Views
claymontgomery
Contributor IV

I use OpenGL ES without X11 extensively on the iMX51, iMX53 and iMX6x.  Did you get it to work?

Are you using the latest 11.09 BSP release from Freescale?

0 Kudos
Reply

3,077 Views
PaulShirren
Contributor I

Brian, did you get an answer to your question. The _fbdev demos aren't initialising for me on my imx53 qsb either.

0 Kudos
Reply

3,077 Views
sidebranch
Contributor II

Can you run an strace to see if there is anything obvious failing?

0 Kudos
Reply

3,077 Views
PhilEndecott
Contributor II
Do the demo programs work for you? See my post here: http://imxcommunity.org/group/imx53quickstartboard/forum/topics/opengl-demo-programs I haven't tried to run my own OpenGL programs yet, but I'm not expecting it to be a smooth process since these demos don't work...
0 Kudos
Reply