One wire problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

One wire problem

1,136件の閲覧回数
sountharya1z
Contributor I
Hi, I am working with 1kb EEPROM DS2431 one wire device in IMX51 processor. By default the processor itself supports one wire. I loaded the slave module first and then the master module. For reading/writing to the device, the 1-wire driver provides a binary attribute inside the sysfs. In the case of the DS2431, this attribute is placed under the following path and with the following attributes ls /sys/devices/w1_bus_master1/bus/devices/2d-0000015db4d0/ The 2d-0000015db4d0 is the unique device id that will appear after the master detects the slave device. In my case I connected two devices in parallel but only one device is detected in sysfs. I googled but I didnt find any clue why the 2nd device is not detected. Did I miss anything? Thanks in advance for your help
タグ(2)
0 件の賞賛
返信
0 返答(返信)