On chip boot ROM decides hid or usb mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On chip boot ROM decides hid or usb mode?

ソリューションへジャンプ
2,898件の閲覧回数
maheshkumarkoda
Contributor III

Hello,

Recently I started working with i.MX6 Quadcore, I am trying to flash Bootloader.

I am getting an error like this ''waiting for u-boot serial console at COM4''.

So, I thought there will be either a problem with U-boot or with COM port (COM4 in my case).

To check U-boot problem - i tried flashing U-boot files (.bin & .uimage files) using MfgTool and the flash is successful.

Here I found while flashing using MfgTool the USB is in HID mode(Human Interface Device).

So I'm suspecting a problem with COM port, when i checked ref doc i found Boot ROM puts serial downloader into HID mode to flash.

My question is how can i put serial downloader into COM mode instead of HID mode?

Please help asap.

Thanks inadvance.

ラベル(3)
1 解決策
2,631件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

iROM can not change to "COM mode", because its behaviour is hardcoded,

can not be changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,632件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

iROM can not change to "COM mode", because its behaviour is hardcoded,

can not be changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------