OTG connection when used as device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTG connection when used as device

1,033 Views
vigneshvasudeva
Contributor II

I am using I.MX6 in one of my boards, I believe the USB_OTG_VBUS(pin E9) of I.MX6 need not be connected to 1st pin of OTG connector if I.MX6 OTG is intended to be used as device.

Only the data lines and GND connection is sufficient for communication, isnt?

Please let me know whether my understanding is correct.

Labels (1)
0 Kudos
Reply
1 Reply

851 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vignesh

yes this is correct, in general VBUS is not needed for normal operation

of i.MX6 USB module. However in any way voltage should be provided to LDO_USB,

using one of two signals: USB_HI_VBUS or USB_OTG_VBUS

Figure 50-1. Power system overview IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply