OPTEE on iMX6UL-EVKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OPTEE on iMX6UL-EVKB

2,016 Views
mikecarlos
Contributor I

Hi,

I recently bought  MCIMX6UL-EVKB . An sdcard image (L4.19.35_1.1.0_MX6UL7D) can be downloaded from NXP and burned to the SD card and it works OK.

However my purpose is to build u-boot, Linux Kernel, optee from source. I have came across few sites explaining how to do it but I could not succeed in getting it running. They all lack a complete instructions perhaps assuming it is already known. I mainly followed this. However since I am a beginner I can not succeed in getting it running. 

I compiled u-boot with: 

make ARCH=arm mx6ul_14x14_evk_optee_defconfig

I formatted the sdcard. I burnt the image to the sd card.

I compiled Linux with: 

make ARCH=arm imx_v7_defconfig

I compiled optee-os which outputs tee.bin which is converted to another binary with some commands.

I am not sure whether to copy this to the sdcard or not.

I have no idea what to write to the rootfs partition of the sdcard.

The device boots but fails to boot properly while the console says

Internal error: Oops - bad mode: 0 [#1] PREEMPT SMP ARM

I have spent quite a time trying to succeed. I understand there are quite a lot of resources on the internet but I can say that the ones I could reach are not very helpful.  My actual question is: are there any complete tutorial explaining step by step  for beginners how to build Linux with optee on imx6ul-evkb?

Regards

Labels (3)
0 Kudos
Reply
3 Replies

1,923 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

OP-TEE OS is required on the boot partition with the TEE file for OP-TEE enablement

0 Kudos
Reply

1,923 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can try to refer to this thread https://community.nxp.com/docs/DOC-344453 

0 Kudos
Reply

1,719 Views
008kai
Contributor II

Hello, we do not have permission to obtain this file

0 Kudos
Reply