OPENCL clBuildProgram fails with no return

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OPENCL clBuildProgram fails with no return

4,116件の閲覧回数
mauromanzo
Contributor I

Hi to all,

I have a Udoo Quad board with the i.mx6Quad CPU and the Vivante GC2000 GPU. The OS is UDOObuntu, that essentially is an Ubuntu 12.04 based distro.

In CodeBlocks I'm trying to run a simple "helloWorld" OpenCL program. The program is built and the libraries are linked, but at runtime there is a strange error after calling "clBuildProgram".

The kernel computes a simple C=A+B vector sum:

__kernel void hello_kernel(__global const float *a,__global const float *b,__global float *result)

{

     int gid = get_global_id(0);

     result[gid] = a[gid] + b[gid];

}

The C++ file is very simple. I'll show only the function that should create and build the CL program;

cl_program CreateProgram(cl_context context, cl_device_id device, const char* fileName)

{

    cl_int errNum = -1000;

    cl_program program;

    std::ifstream kernelFile(fileName, std::ios::in);

    if (!kernelFile.is_open())

    {

        std::cerr << "Failed to open file for reading: " << fileName << std::endl;

        return NULL;

    }

    std::ostringstream oss;

    oss << kernelFile.rdbuf();

    std::string srcStdStr = oss.str();

    const char *srcStr = srcStdStr.c_str();

    program = clCreateProgramWithSource(context, 1,(const char**)&srcStr,NULL, NULL);

    if (program == NULL)

    {

        std::cerr << "Failed to create CL program from source." << std::endl;

        return NULL;

    }

    ///////////////////// ERROR IS HERE //////////////////////

    try

    {

      //errNum = clBuildProgram(program, 1, &device, "-cl-std=CL1.1 -w -cl-opt-disable", NULL, NULL);

        errNum = clBuildProgram(program, 0, NULL, "", NULL, NULL);

    } catch(...)

    {

        std::cout<< __LINE__<<", "<<__FILE__<<": errNum="<<errNum<<std::endl;

    }

    std::cout<< __LINE__<<", "<<__FILE__<<": errNum="<<errNum<<std::endl;

    if (errNum != CL_SUCCESS)

    {

        // Determine the reason for the error

        size_t logSize;

        clGetProgramBuildInfo(program, device, CL_PROGRAM_BUILD_LOG,0, NULL, &logSize);

        char* buildLog = new char[logSize];

        clGetProgramBuildInfo(program, device, CL_PROGRAM_BUILD_LOG,sizeof(buildLog), buildLog, NULL);

        std::cerr << "Error in kernel: " << std::endl;

        std::cerr << buildLog;

        clReleaseProgram(program);

        delete[] buildLog;

        return NULL;

    }

    return program;

}

Both the version in line 29 and the version in line 30 crash. The catch block is never reached, and the program exits immediately.

The compiler options are:

-march=native -fexceptions -DLINUX -DUSE_SOC_MX6 -Wall  -fsigned-char  -mfloat-abi=hard -mfpu=neon -DEGL_API_FB -DGPU_TYPE_VIV -DGL_GLEXT_PROTOTYPES -DENABLE_GPU_RENDER_20

I'm linking glib2.0, OpenCL, GAL, CLC, dl and pthread. Also the linker has option -mfloat-abi=hard

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

3,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mauro

you can try Freescale OpenCL Hello World example for Sabre boards

https://community.freescale.com/docs/DOC-93984

L3.0.35_4.1.0_UBUNTU_RFS_BSP

as for Udoo board, one can post on meta-fsl-arm mailing list,

so that someone familiar with that board could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 件の賞賛
返信

3,126件の閲覧回数
mauromanzo
Contributor I

Hi Igor,

I tried also with the Freescale "Hello World". The options given to compiler and linker are taken from it. Unfortunately I had the same error.

The only difference is that I used the libOpenCL.so libGAL.so and libCLC.so already provided in Udoobuntu image inside /usr/lib/.

In fact I could not compile LTIB as explained in Freescale documentation.

Could the problem be a wrong version of the OpenCL libraries? If so, is there a link where to download the correct ones without working on LTIB?

Thanks,

Mauro

0 件の賞賛
返信

3,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mauro

yes these may depend on libraries versions.

I am not familiar with Udoo distributions, suggest to post

on Udoo forum or meta-fsl-arm mailing list.

~igor

0 件の賞賛
返信