i.MX6SoloLite EVK can't boot from emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SoloLite EVK can't boot from emmc

702 Views
darrenjiao
Contributor I

hi anyone,

i used the target board MCIMX6SLEVK board and the linux refer docs(i.MX_6SoloLite_EVK_Linux_User's_Guide.pdf) build image to boot from SD2 by emmc device.

Used micron emmc device mount the rootfs read only and used greenliant emmc device can't mount rootfs.

used microSD card will mount rootfs read only.

Labels (2)
0 Kudos
Reply
1 Reply

511 Views
igorpadykov
NXP Employee
NXP Employee

Hi Darren

probably you can look below

Read-only Root Filesystem - Linux Pendrive

btw what is about Demo images, are they working fine ?

L3.0.35_4.1.0_DEMO_IMAGE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.

Best regards

igor

0 Kudos
Reply