OP-TEE with Secure Storage RPMB support on iMx8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OP-TEE with Secure Storage RPMB support on iMx8QM

3,443件の閲覧回数
matteo-facchinetti
Contributor II

Hi,

On iMx8QM, I need to use OP-TEE with the Secure Storage RPMB. I have turned on the related config options and it seems work properly.

Now, I want to implement also the tee_otp_get_hw_unique_key() and my strategy is to implements a MKVB module which retrieves the HUK, similar to has already done on iMx6.

https://github.com/OP-TEE/optee_os/pull/3608/commits/df90b3e278b4ee5b0216a7536b7b33fefa8f3e8c

Is this code useful also with the CAAM on  imx8QM?

Idea is to turn on CAAM module porting this series of patches
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enable-CAAM-accelerating-in-OP-TEE-on-i-...
and then use the code mentioned above to retrive the HUK.

Is this feasible? or there is something that I have not considered.

All opinions are welcome!!!

Thanx in advance,

Matteo

0 件の賞賛
返信
1 返信

3,409件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信