OMXPlayer Library issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OMXPlayer Library issue

5,759件の閲覧回数
ThanarajS
Contributor III

 

Hi all,

While playing stream from media player, we are observing the following issue. Please help us to get identify where is the problem?

07-27 09:48:17.682 2309 3166 I OMXPlayer: Loading content: sharedfd://30:0:240724:0
07-27 09:48:17.682 2309 3166 I OMXPlayer: LEVEL: 1 FUNCTION: MediaTypeInspect LINE: 1655
07-27 09:48:17.682 2309 3166 I OMXPlayer: Can't inspect media content type by subfix.
07-27 09:48:17.712 2309 19209 I OMXPlayer: LEVEL: 1 FUNCTION: prepare LINE: 422
07-27 09:48:17.712 2309 19209 I OMXPlayer: failed to open file: /data/system/audio_pass_through_pref.
07-27 09:48:17.742 2309 19210 I OMXPlayer: nPreCacheSize = 120362
07-27 09:48:17.752 2309 2696 I OMXPlayer: start player.
07-27 09:48:20.802 2309 19208 I OMXPlayer: Pause player.
07-27 09:48:50.352 2309 2696 I OMXPlayer: Stop Player.
07-27 09:48:50.392 2309 2696 I OMXPlayer: Loading content: sharedfd://30:0:240724:0
07-27 09:48:50.392 2309 2696 I OMXPlayer: LEVEL: 1 FUNCTION: MediaTypeInspect LINE: 1655
07-27 09:48:50.392 2309 2696 I OMXPlayer: Can't inspect media content type by subfix.
07-27 09:48:50.422 2309 19281 I OMXPlayer: LEVEL: 1 FUNCTION: prepare LINE: 422
07-27 09:48:50.422 2309 19281 I OMXPlayer: failed to open file: /data/system/audio_pass_through_pref.
07-27 09:48:50.442 2309 19282 I OMXPlayer: nPreCacheSize = 120362
07-27 09:48:50.452 2309 3166 I OMXPlayer: start player.
07-27 09:48:53.502 2309 19280 I OMXPlayer: Pause player.
07-27 09:51:13.022 2309 2309 I OMXPlayer: Stop Player.
07-27 09:51:13.062 2309 2309 I OMXPlayer: Loading content: sharedfd://30:0:240724:0
07-27 09:51:13.062 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: MediaTypeInspect LINE: 1655
07-27 09:51:13.062 2309 2309 I OMXPlayer: Can't inspect media content type by subfix.
07-27 09:51:13.102 2309 19544 I OMXPlayer: LEVEL: 1 FUNCTION: prepare LINE: 422
07-27 09:51:13.102 2309 19544 I OMXPlayer: failed to open file: /data/system/audio_pass_through_pref.
07-27 09:51:13.122 2309 19545 I OMXPlayer: nPreCacheSize = 120362
07-27 09:51:13.142 2309 2696 I OMXPlayer: start player.
07-27 09:52:09.792 2309 2309 I OMXPlayer: Stop Player.
07-27 09:52:11.822 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: WaitCommand LINE: 1060
07-27 09:52:11.822 2309 2309 I OMXPlayer: OMX.Freescale.std.audio_render.android.sw-based wait command[0:4] timeout.
07-27 09:52:12.352 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: SendCommand LINE: 1004
07-27 09:52:12.352 2309 2309 I OMXPlayer: OMX.Freescale.std.audio_render.android.sw-based send command[0:2] timeout.
07-27 09:52:12.352 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: DoExec2Idle LINE: 1182
07-27 09:52:12.352 2309 2309 I OMXPlayer: State trans to 2 failed.
07-27 09:52:12.882 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: SendCommand LINE: 985
07-27 09:52:12.882 2309 2309 I OMXPlayer: OMX.Freescale.std.audio_render.android.sw-based Time out for Sending Command [2:1], Busy on Command [0:2].
07-27 09:52:12.882 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: WaitCommand LINE: 1038
07-27 09:52:12.882 2309 2309 I OMXPlayer: OMX.Freescale.std.audio_render.android.sw-based Wait incorrect Command[2:1], ProcessingCmd is [0:2].
07-27 09:52:13.892 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: WaitCommand LINE: 1060
07-27 09:52:13.892 2309 2309 I OMXPlayer: OMX.Freescale.std.clocksrc.sw-based wait command[2:0] timeout.
07-27 09:52:13.892 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: OMX_SetupTunnel LINE: 512
07-27 09:52:13.892 2309 2309 I OMXPlayer: OMX setup tunnel fail.
07-27 09:52:13.892 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: OMX_SetupTunnel LINE: 512
07-27 09:52:13.892 2309 2309 I OMXPlayer: OMX setup tunnel fail.
07-27 09:52:14.412 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: SendCommand LINE: 1004
07-27 09:52:14.412 2309 2309 I OMXPlayer: OMX.Freescale.std.clocksrc.sw-based send command[0:2] timeout.
07-27 09:52:14.412 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: DoExec2Idle LINE: 1182
07-27 09:52:14.412 2309 2309 I OMXPlayer: State trans to 2 failed.
07-27 09:52:14.412 2309 2309 I OMXPlayer: LEVEL: 1 FUNCTION: StateTransDownWard LINE: 336
07-27 09:52:14.412 2309 2309 I OMXPlayer: OMX.Freescale.std.clocksrc.sw-based Invalid state transitioin: 4 -> 1.

Regards,
Thanaraj Subramani
0 件の賞賛
返信
4 返答(返信)

5,754件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Thanaraj

 

probably omxplayer is wrongly installed, one can check below link, select processor and test

Demo Umage on NXP reference board. Supported codecs are described in Release Notes

included in documentation package for each release

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Best regards
igor

0 件の賞賛
返信

5,748件の閲覧回数
ThanarajS
Contributor III

Hi Igor,

I didn't install OMXPlayer library separately. It comes with android. I am using android-4.2.2-r1 version. is there any issue in that android specific version related to OMXPlayer library? 

In what kind of scenarios, that above issue will be occured?..please give some points because I am not familier with android/external/fsl_imx_omx package.

Regards,
Thanaraj Subramani
0 件の賞賛
返信

5,731件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Thanaraj

 

in old android versions omxplayer is provided as separate  "Extended Codec" package

as described in attached documents.

 

Best regards
igor

 

0 件の賞賛
返信

5,747件の閲覧回数
ThanarajS
Contributor III
 
Regards,
Thanaraj Subramani
0 件の賞賛
返信