OK8MP-C camera Image missing line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OK8MP-C camera Image missing line

1,683 次查看
zhichao_hu
Contributor I
I can use imx8 to obtain the image successfully, but the original image(yuv422-8bit) has problems such as missing lines and wrong line positions. Has anyone encountered similar problems?
 
This camera is ti964, and the camera register configuration is normal. I can read from the 964 chip that the output rows and columns are consistent with those of the camera.
 

Is there any way to help me locate this problem? I don't know what caused the error of the original data line of the image

0 项奖励
回复
4 回复数

1,636 次查看
zhichao_hu
Contributor I

Thanks, I have solved this problem

0 项奖励
回复

1,679 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you use 8QM board? and which dts file do you use? how did you change it? pls send the patch to check

0 项奖励
回复

1,676 次查看
zhichao_hu
Contributor I

I use forlinx imx8MP OKMX8MP-C.

I change dts i2c2 part ov5645 to :

&i2c2 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2>;
status = "okay";

jh1mp_0: jh1mp_mipi1@32 {
compatible = "ti,jh1mp";
reg = <0x32>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_csi0_pwn>, <&pinctrl_csi0_rst>;
clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
clock-names = "xclk";
assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
assigned-clock-parents = <&clk IMX8MP_SYS_PLL2_200M>;
assigned-clock-rates = <20000000>;
csi_id = <0>;
enable-gpios = <&gpio3 20 GPIO_ACTIVE_HIGH>;
reset-gpios = <&gpio3 19 GPIO_ACTIVE_LOW>;
clock-frequency = <20000000>;
mclk = <20000000>;
mclk_source = <0>;
mipi_csi;
virtual-channel;
status = "okay";

port {
jh1mp_mipi_0_ep: endpoint {
remote-endpoint = <&mipi_csi0_ep>;
data-lanes = <1 2 3 4>;
clock-lanes = <0>;
link-frequencies = /bits/ 64 <336000000>;
};
};
};
};
0 项奖励
回复

1,642 次查看
joanxie
NXP TechSupport
NXP TechSupport

what do you mean "I can use imx8 to obtain the image successfull"? this isn't nxp board, what bsp version do you use? did you have any logfile to share?

0 项奖励
回复