HI,
I read in the manual (IMX6DQRM) that " Memory alias is also supported for on-chip RAM. Address from 0x00940000 to
0x009FFFFF are alias addresses for it, any read/write operation to this area will be mapped back to the 256 Kbytes area.". How is this mapped? I mean, the OCRAM is 0.25MB and the alias memory is 0.75MB. Is there 3 address location, that may be mapped to the OCRAM area? 
Regards,
Ajmal
解決済! 解決策の投稿を見る。
Not something I have looked at before, but it should be very easy to test/verify.
From the description I would expect there are four regions all identical -
0x00900000 - 0x0093ffff
0x00940000 - 0x0097ffff
0x00980000 - 0x009bffff
0x009c0000 - 0x009fffff
You should be able to test this quickly with a debugger or uboot (mm, md commands).
Regards
Ross
Not something I have looked at before, but it should be very easy to test/verify.
From the description I would expect there are four regions all identical -
0x00900000 - 0x0093ffff
0x00940000 - 0x0097ffff
0x00980000 - 0x009bffff
0x009c0000 - 0x009fffff
You should be able to test this quickly with a debugger or uboot (mm, md commands).
Regards
Ross