OBDS test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OBDS test

1,559件の閲覧回数
sachusanal
Contributor III

Hai Sir ,

let me know in OBDS test we can perform the touch screen test.

is it possible means help me... and send me the OBDs source code for touch

i am using IMX6qsabre sd board

ラベル(1)
0 件の賞賛
返信
1 返信

1,416件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sachu

I am afraid there is no full touch screen test, first

one can look at p1003 commands

Re: IPU Usage on IMX6 processor..

i.MX 6Series Platform SDK  : Bare-metal SDK for the i.MX6

has only i2c_device_id_check_p1003_tsc.c

examples of various touch screen usage

http://boundarydevices.com/tag/touch-screen/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信