Not possible to compile the generated code on CM4 using Azure RTOS and uart driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not possible to compile the generated code on CM4 using Azure RTOS and uart driver

ソリューションへジャンプ
1,649件の閲覧回数
Mc2023
Contributor IV

Hello all,

I have bought MIMXRT1160-EVK. So I am new with this EVK and MCUXpresso IDE.

I have created  a project with the SDK Wizard for CM7 composed of the Azure RTOS and the uart driver. I can compile the generated code and I can run it. Everything looks fine.

However, now, if I do exactly the same thing but I select CM4 as standalone. Then I compile the generated code, errors are displayed.

Could you tell me why I cannot compile the generated code with CM4? Thanks in advance!

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,607件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I review your questions, unfortunately, there is no information about that movement.

This is the note app for move the applicacion maybe could help you to undesrtand.
RT-Thread Board Port and Application Development (nxp.com)

Then I recommend using the FreeRTOS examples of CM4 to review how this works and then you could try port again the CM7 azure example to the CM4.

Pavel_Hernandez_0-1677526302597.png

Best regards,
Pavel

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,608件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I review your questions, unfortunately, there is no information about that movement.

This is the note app for move the applicacion maybe could help you to undesrtand.
RT-Thread Board Port and Application Development (nxp.com)

Then I recommend using the FreeRTOS examples of CM4 to review how this works and then you could try port again the CM7 azure example to the CM4.

Pavel_Hernandez_0-1677526302597.png

Best regards,
Pavel

 

0 件の賞賛
返信