Not able to get the source code of kk4.4.3_2.0.0.-ga

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to get the source code of kk4.4.3_2.0.0.-ga

1,208件の閲覧回数
mutyalaraoneela
Contributor III

Hi all,

          I am working on IMX6 solo lite board in order to bring up android 4.4.3 on it. I am following the user guide document for downloading the source code , kernal source and uboot source.I am able to download the Kernal image and uboot image but not the source code of android. It would be great and helpful to me if any reply.

Thank you,

Mutyala Rao.

0 件の賞賛
返信
2 返答(返信)

1,079件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Have You tried instructions of section 3.1 [Getting Android source code (Android/kernel/U-Boot)]

of "Android_User's_Guide.pdf"  ?

http://www.freescale.com/webapp/Download?colCode=IMX6_KK443_200_ANDROID_DOCS&Parent_nodeId=133769948...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,079件の閲覧回数
mutyalaraoneela
Contributor III

Hi ,

       I followed user guide,but iam not able to patch.It is showing like

     root@cpu347:~/myandroid# c_patch /opt/android_KK4.4.3_2.0.0-ga_core_source/code/KK4.4.3_2.0.0-ga imx_KK4.4.3_2.0.0-ga
     Error! Can't read base file - /opt/android_KK4.4.3_2.0.0-ga_core_source/code/KK4.4.3_2.0.0-ga/baseversion

     please help me.

Thank you,

Mutyala Rao

0 件の賞賛
返信