Not able to get HDMI interface while booting through TFTP/NFS or SD card boot procedure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to get HDMI interface while booting through TFTP/NFS or SD card boot procedure

1,059 Views
vamsi92
Contributor I

Hi,

 

I am working on Apalis 1.1v IMX 6 board which is placed on Ixora carrier board with Embedded linux BSP version 5 , initially  I tried booting board using Toradex easy installer here I am able to get HDMI interface by default, but when i tried to boot from TFTP/NFS or SD card boot procedures I am not able to get HDMI interface, tried copying overlays folder and overlays.txt file along with kernel and dtb files, though I am not able to get  HDMI interface,I am not able to find HDMI interface dmesg logs also.

 

Please suggest me the procedure to bring up HDMI interface with TFTP/NFS or SD card boot procedures,

 

With Regards,

-Vamsi.

0 Kudos
Reply
1 Reply

1,043 Views
joanxie
NXP TechSupport
NXP TechSupport

could you reproduce this on nxp imx6 board? I can get HDMI interface from sd card boot on nxp imx6q sdb baord before, since you used the third party board, pls contact them to get further help

0 Kudos
Reply