Not able to get HDMI interface while booting through TFTP/NFS or SD card boot procedure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to get HDMI interface while booting through TFTP/NFS or SD card boot procedure

1,078件の閲覧回数
vamsi92
Contributor I

Hi,

 

I am working on Apalis 1.1v IMX 6 board which is placed on Ixora carrier board with Embedded linux BSP version 5 , initially  I tried booting board using Toradex easy installer here I am able to get HDMI interface by default, but when i tried to boot from TFTP/NFS or SD card boot procedures I am not able to get HDMI interface, tried copying overlays folder and overlays.txt file along with kernel and dtb files, though I am not able to get  HDMI interface,I am not able to find HDMI interface dmesg logs also.

 

Please suggest me the procedure to bring up HDMI interface with TFTP/NFS or SD card boot procedures,

 

With Regards,

-Vamsi.

0 件の賞賛
返信
1 返信

1,062件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you reproduce this on nxp imx6 board? I can get HDMI interface from sd card boot on nxp imx6q sdb baord before, since you used the third party board, pls contact them to get further help

0 件の賞賛
返信