Non-functional machine config for imx8mqevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Non-functional machine config for imx8mqevk

1,544 Views
thomaskoeller
Contributor I

Hi,

I am trying to build the imx8mqevk BSP using the meta-freescale layer from the yocto zeus branch. There is a machine configuration for this target in meta-freescale/conf/machine/imx8mqevk.conf, but using this file results in a compilation error when building the linux-imx_5.4 kernel recipe:

| make[2]: *** No rule to make target 'arch/arm64/boot/dts/freescale/fsl-imx8mq-evk.dtb'. Stop.
| /home/tkoeller/imx-manifest/build/tmp/work-shared/imx8mqevk-basler/kernel-source/Makefile:1243: recipe for target 'freescale/fsl-imx8mq-evk.dtb' failed
| make[1]: *** [freescale/fsl-imx8mq-evk.dtb] Error 2
| /home/tkoeller/imx-manifest/build/tmp/work-shared/imx8mqevk-basler/kernel-source/Makefile:179: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2

This is because the file name 'fsl-imx8mq-evk.dtb' is wrong, it should be 'imx8mq-evk.dtb', without the 'fsl-' prefix. The machine configuration files in the new meta-imx layer correctly reflect the device tree name changes, unfortunatly, there is no machine configuration for imx8mqevk in this layer.

0 Kudos
Reply
2 Replies

1,463 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Thomas Koeller,

Would you please confirm which BSP you are using? Are you using one of the BSP Releases or the Community BSP?

I would recommend using the BSP Release L5.4.3_1.0.0 if possible (which is based in Zeus).

 Regards,

0 Kudos
Reply

1,463 Views
thomaskoeller
Contributor I

Thank you - I will try that.

regards,

Thomas

Thomas Koeller

Senior Software Developer

<https://www.baslerweb.com/?utm_medium=email&utm_source=basler-internal&utm_content=basler%20logo>

Basler AG

An der Strusbek 60-62

22926 Ahrensburg

Germany

Tel. +49 4102 463 390

Fax +49 4102 463 46 390

Thomas.Koeller@baslerweb.com

<http://www.baslerweb.com>www.baslerweb.com<http://www.baslerweb.com>

<http://www.facebook.com/BaslerAG> <https://twitter.com/Basler_AG> <https://www.linkedin.com/company/basler-ag> <http://www.kununu.com/de/all/de/it/basler> <http://www.youtube.com/user/BaslerAG> <https://www.xing.com/companies/baslerag> -[https://www.baslerweb.com/baslermedia/socialmediaicons_email_signature/imaginghub_blue.gif]<https://imaginghub.com/partners/category-hardware/51-basler-ag>

Vorstand: Dr.-Ing. Dietmar Ley (Vorsitzender) · John P. Jennings · Arndt Bake · Hardy Mehl

Aufsichtsratsvorsitzender: Norbert Basler

Basler AG · Amtsgericht Lübeck HRB 4090 · Ust-IdNr.: DE 135 098 121 · Steuer-Nr.: 30 292 04497 · WEEE-Reg.-Nr. DE 83888045

0 Kudos
Reply