Nobody Cared issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nobody Cared issue

Jump to solution
4,455 Views
Raana
Contributor III

Hi,

Currently I am working on imx6DL processor (i.MX6Q/D/S)

Once Linux is launched,

If we are not doing anything on the board, after some times it's showing the below print but console is there.


root@iWave-G15S-SBC ~$ irq 402: nobody cared (try booting with the "irqpoll" option)

[<80045cd4>] (unwind_backtrace+0x0/0xf8) from [<800a5fec>] (__report_bad_irq+0x28/0xc4)

[<800a5fec>] (__report_bad_irq+0x28/0xc4) from [<800a6330>] (note_interrupt+0x1e4/0x240)

[<800a6330>] (note_interrupt+0x1e4/0x240) from [<800a51d4>] (irq_thread+0x1c4/0x1fc)

[<800a51d4>] (irq_thread+0x1c4/0x1fc) from [<80089468>] (kthread+0x80/0x88)

[<80089468>] (kthread+0x80/0x88) from [<8003fa64>] (kernel_thread_exit+0x0/0x8)

handlers:

[<800a49b0>] irq_default_primary_handler threaded [<802a1ec0>] pfuze_irq_thread

Disabling IRQ #402

root@iWave-G15S-SBC ~$

root@iWave-G15S-SBC ~$

root@iWave-G15S-SBC ~$


Is this an issue ??

How to recover from this ??


NOTE:

In my point of view, this issue is coming from PMIC, because irq 402 is for PMIC only


Thanks in Advance

Best Regards,

J.P.Raja

Labels (1)
0 Kudos
Reply
1 Solution
3,904 Views
weidong_sun
NXP TechSupport
NXP TechSupport

ok, Raana,

     It means that PMIC interrupt on cusotmer board is not different from that of FSL Evk board,So you ajusted PMIC interrupt to be GPIO_7_13(customer uses it) , then the issue is resovled.

    Rgiht ?

Regards,

Weidong

View solution in original post

0 Kudos
Reply
6 Replies
3,905 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Raana,

      Please tell us which board you are using ? Is it our MX6 Dual Lite SABRE AI CPU Card ?

Regards,

Weidong

0 Kudos
Reply
3,905 Views
Raana
Contributor III

Hi weidong,

Thanks for your quick response.

     Currently I am using imx6 Dual lite/solo SabreSD based custom board

Regards,

Raana

0 Kudos
Reply
3,905 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Raana,

      Is the PMIC MMPF0100 ? Could you tell me which GPIO pin pmic's INT is connected to ?

Regards,

Weidong

0 Kudos
Reply
3,905 Views
Raana
Contributor III

Hi Weidong,

     No, I am using Freescale PMIC (pfuze100)

Issue solved after configuring the proper PMIC interrupt GPIO (GPIO_7_13).

Thanks for your support

Regards,

J.P.Raja

0 Kudos
Reply
3,905 Views
weidong_sun
NXP TechSupport
NXP TechSupport

ok, Raana,

     It means that PMIC interrupt on cusotmer board is not different from that of FSL Evk board,So you ajusted PMIC interrupt to be GPIO_7_13(customer uses it) , then the issue is resovled.

    Rgiht ?

Regards,

Weidong

0 Kudos
Reply
3,905 Views
Raana
Contributor III

Yes, Weidong,

          PMIC interuupt GPIO of the Customer board is also same as EVK board.

So, the Issue solved, after configuring the proper PMIC interrupt GPIO (GPIO_7_13) pin.

Thanks for your support

Regards,

J.P.Raja

0 Kudos
Reply