No space left on device errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No space left on device errors

ソリューションへジャンプ
6,412件の閲覧回数
neo1
Contributor II

cp: writing `/mnt/rwfs/var/lib/rpm/Filemd5s': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Installtid': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Basenames': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Group': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Sha1header': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Triggername': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Packages': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Conflictname': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Providename': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Sigmd5': No space left on device

cp: writing `/mnt/rwfs/var/state/dhcp/dhcpd.leases': No space left on device

cp: writing `/mnt/rwfs/var/state/dhcp/dhclient.leases': No space left on device

cp: writing `/mnt/rwfs/var/www/cgi-bin/test_cgi': No space left on device

cp: writing `/mnt/rwfs/var/www/html/index.html': No space left on device

cp: writing `/mnt/rwfs/var/run/utmp': No space left on device

cp: writing `/mnt/rwfs/var/log/wtmp': No space left on device

.

.

.

rebuilding rpm database

rpmdb: write: 0xbee8f524, 8192: No space left on device

error: db4 error(28) from dbenv->open: No space left on device

error: cannot open Packages index

I get these errors in the bootup logs. My SD card has lots of free space but these messages come up everytime on boot up. Any idea why?

Im using im35 based custom board running  Linux-2.6.31

$ uname -a

Linux freescale 2.6.31-207-g7286c01-svn1013 #66 Tue May 28 10:56:29 PDT 2013 armv6l GNU/Linux

ラベル(1)
タグ(1)
1 解決策
4,324件の閲覧回数
neo1
Contributor II

Solution:

In /etc/rc.d/rc.conf

change the following line:

export TMPFS_SIZE="512k" to export TMPFS_SIZE="4m"

元の投稿で解決策を見る

2 返答(返信)
4,324件の閲覧回数
LeonardoSandova
Specialist I

Perhaps the folder /mnt/rwfs is not mounted so you get those errors. Try creating a partition on your SD and mount this folder on this new partition.

Leo

0 件の賞賛
返信
4,325件の閲覧回数
neo1
Contributor II

Solution:

In /etc/rc.d/rc.conf

change the following line:

export TMPFS_SIZE="512k" to export TMPFS_SIZE="4m"