Hi,
I am trying to use wm8731 codec with i.MX6UL.
The wm8731 codec is on a MIKROE-506 proto board and is wired this way for the SAI part :
imx6ul <=> MIKROE-506 <=> wm8731
CSI_D6 (SAI1_RX_DATA) MISO ADCDAT
CSI_D2 (SAI1_RX_SYNC) ADCL ADCLRC
CSI_D3 (SAI1_RX_BCLK) SCK BCLK
CSI_D7 (SAI1_TX_DATA) MOSI DACDAT
CSI_D4 (SAI1_TX_SYNC) DACL DACLRC
CSI_D1 (SAI1_MCLK) SCK BCLK
The I2C wiring is OK, I am able to send control command to the codec, for example I can make a loop between microphone and HP with amixer.
I'm using linux 4.8.10 and the here is the relevant parts of the device tree :
sound {
compatible = "simple-audio-card";
simple-audio-card,model = "wm8731-audio";
simple-audio-card,format = "i2s";
simple-audio-card,audio-routing =
"Line Out", "LOUT",
"Line Out", "ROUT",
"Headphone Jack", "RHPOUT",
"Headphone Jack", "LHPOUT",
"LLINEIN","Line In",
"RLINEIN","Line In";
simple-audio-card,cpu {
sound-dai = <&sai1>;
bitclock-master;
frame-master;
};
simple-audio-card,codec {
sound-dai = <&codec>;
};
};
&sai1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1>;
assigned-clocks = <&clks IMX6UL_CLK_SAI1_SEL>,<&clks IMX6UL_CLK_SAI1>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>,<12288000>,<11289600>;
status = "okay";
};
&i2c1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1>;
clock_frequency = <400000>;
status = "okay";
};
pinctrl_sai1: sai1grp {
fsl,pins = <
MX6UL_PAD_CSI_DATA05__SAI1_TX_BCLK 0x17088
MX6UL_PAD_CSI_DATA03__SAI1_RX_BCLK 0x17088
MX6UL_PAD_CSI_DATA04__SAI1_TX_SYNC 0x17088
MX6UL_PAD_CSI_DATA02__SAI1_RX_SYNC 0x17088
MX6UL_PAD_CSI_DATA07__SAI1_TX_DATA 0x11088
MX6UL_PAD_CSI_DATA06__SAI1_RX_DATA 0x11088
MX6UL_PAD_JTAG_TMS__CCM_CLKO1 0x17088
>;
};
When trying to play a sound with aplay, I can hear the codec sending some kind of noise during aplay execution but nothing related with the sound I am trying to play.
I am really not sure with the sai1grp part of the device tree.
Any help will be really appreciated.
Regards
Yann
Hi,
I'm facing this same problem with my VARISCITE DART6 UL based on i.MX 6UL.
DTSI configuration file seems to be OK. Connection for analog audio is OK (pins are HPROUT and HPLOUT).
Cheking on the evaluation board VAR-6UL (made by VARISCITE) and launch "aplay" command from terminal, sound regularly comes from the headphones socket.
Thus: board configuration and hardware connection seem to be OK. Whatelse trial or check could I perform in order to go on?
Hello Yann,
The latest linux BSP released by NXP is Linux 4.1.15_2.0.0 BSP, but your kernel is 4.8, so we have no way to support you!
Best Regards,
weidong