No rootfs.ext3 in /tmp/deploy/images/<board>

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No rootfs.ext3 in /tmp/deploy/images/<board>

1,429 Views
husnain_kazmi
Contributor I

Hi,

I built the Yocto image using Yocto Training - HOME 

It states that I should have a rootfs.ext3 in /tmp/deploy/images/<board>folder. However, I don't have any such thing. The contents of this folder are:

drwxr-xr-x 2 kazmi kazmi 4096 Jan 18 12:40 ./
drwxrwxr-x 3 kazmi kazmi 4096 Jan 17 22:20 ../
-rw-r--r-- 2 kazmi kazmi 12135 Jan 17 22:34 core-image-base-imx6qdlsabreauto-20190117131043.rootfs.manifest
-rw-r--r-- 1 kazmi kazmi 143864832 Jan 17 22:40 core-image-base-imx6qdlsabreauto-20190117131043.rootfs.wic
-rw-r--r-- 2 kazmi kazmi 31781772 Jan 17 22:40 core-image-base-imx6qdlsabreauto-20190117131043.rootfs.wic.gz
-rw-r--r-- 1 kazmi kazmi 135520 Jan 17 22:34 core-image-base-imx6qdlsabreauto-20190117131043.testdata.json
lrwxrwxrwx 2 kazmi kazmi 63 Jan 17 22:34 core-image-base-imx6qdlsabreauto.manifest -> core-image-base-imx6qdlsabreauto-20190117131043.rootfs.manifest
lrwxrwxrwx 1 kazmi kazmi 61 Jan 17 22:34 core-image-base-imx6qdlsabreauto.testdata.json -> core-image-base-imx6qdlsabreauto-20190117131043.testdata.json
lrwxrwxrwx 2 kazmi kazmi 61 Jan 17 22:40 core-image-base-imx6qdlsabreauto.wic.gz -> core-image-base-imx6qdlsabreauto-20190117131043.rootfs.wic.gz
lrwxrwxrwx 2 kazmi kazmi 72 Jan 17 22:20 imx6dl-sabreauto.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 78 Jan 17 22:20 imx6dl-sabreauto-ecspi.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-ecspi-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 80 Jan 17 22:20 imx6dl-sabreauto-enetirq.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-enetirq-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 81 Jan 17 22:20 imx6dl-sabreauto-flexcan1.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-flexcan1-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 82 Jan 17 22:20 imx6dl-sabreauto-gpmi-weim.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-gpmi-weim-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 72 Jan 17 22:20 imx6qp-sabreauto.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 78 Jan 17 22:20 imx6qp-sabreauto-ecspi.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-ecspi-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 81 Jan 17 22:20 imx6qp-sabreauto-flexcan1.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-flexcan1-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 82 Jan 17 22:20 imx6qp-sabreauto-gpmi-weim.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-gpmi-weim-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 71 Jan 17 22:20 imx6q-sabreauto.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 77 Jan 17 22:20 imx6q-sabreauto-ecspi.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-ecspi-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 79 Jan 17 22:20 imx6q-sabreauto-enetirq.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-enetirq-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 80 Jan 17 22:20 imx6q-sabreauto-flexcan1.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-flexcan1-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 81 Jan 17 22:20 imx6q-sabreauto-gpmi-weim.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-gpmi-weim-20190117131043.dtb
-rw-rw-r-- 2 kazmi kazmi 853754 Jan 17 22:20 modules--4.1-2.0.x+git0+6c1ad49339-r0-imx6qdlsabreauto-20190117131043.tgz
lrwxrwxrwx 2 kazmi kazmi 73 Jan 17 22:20 modules-imx6qdlsabreauto.tgz -> modules--4.1-2.0.x+git0+6c1ad49339-r0-imx6qdlsabreauto-20190117131043.tgz
lrwxrwxrwx 2 kazmi kazmi 54 Jan 17 22:36 SPL -> SPL-imx6qdlsabreauto-v2017.11+gitAUTOINC+a07698f0bf-r0
lrwxrwxrwx 2 kazmi kazmi 54 Jan 17 22:36 SPL-imx6qdlsabreauto -> SPL-imx6qdlsabreauto-v2017.11+gitAUTOINC+a07698f0bf-r0
-rw-r--r-- 2 kazmi kazmi 39936 Jan 17 22:36 SPL-imx6qdlsabreauto-v2017.11+gitAUTOINC+a07698f0bf-r0
lrwxrwxrwx 2 kazmi kazmi 61 Jan 17 22:36 u-boot.img -> u-boot-imx6qdlsabreauto-v2017.11+gitAUTOINC+a07698f0bf-r0.img
lrwxrwxrwx 2 kazmi kazmi 61 Jan 17 22:36 u-boot-imx6qdlsabreauto.img -> u-boot-imx6qdlsabreauto-v2017.11+gitAUTOINC+a07698f0bf-r0.img
-rw-r--r-- 2 kazmi kazmi 436408 Jan 17 22:36 u-boot-imx6qdlsabreauto-v2017.11+gitAUTOINC+a07698f0bf-r0.img
lrwxrwxrwx 2 kazmi kazmi 72 Jan 17 22:20 zImage -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qdlsabreauto-20190117131043.bin
-rw-r--r-- 2 kazmi kazmi 45914 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 45974 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-ecspi-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 45950 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-enetirq-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 45914 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-flexcan1-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 45970 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-gpmi-weim-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 7473592 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qdlsabreauto-20190117131043.bin
-rw-r--r-- 2 kazmi kazmi 49128 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 49188 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-ecspi-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 49128 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-flexcan1-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 49188 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-gpmi-weim-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 47167 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 47227 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-ecspi-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 47203 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-enetirq-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 47167 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-flexcan1-20190117131043.dtb
-rw-r--r-- 2 kazmi kazmi 47223 Jan 17 22:20 zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-gpmi-weim-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 72 Jan 17 22:20 zImage-imx6dl-sabreauto.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 78 Jan 17 22:20 zImage-imx6dl-sabreauto-ecspi.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-ecspi-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 80 Jan 17 22:20 zImage-imx6dl-sabreauto-enetirq.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-enetirq-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 81 Jan 17 22:20 zImage-imx6dl-sabreauto-flexcan1.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-flexcan1-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 82 Jan 17 22:20 zImage-imx6dl-sabreauto-gpmi-weim.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6dl-sabreauto-gpmi-weim-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 72 Jan 17 22:20 zImage-imx6qdlsabreauto.bin -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qdlsabreauto-20190117131043.bin
lrwxrwxrwx 2 kazmi kazmi 72 Jan 17 22:20 zImage-imx6qp-sabreauto.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 78 Jan 17 22:20 zImage-imx6qp-sabreauto-ecspi.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-ecspi-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 81 Jan 17 22:20 zImage-imx6qp-sabreauto-flexcan1.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-flexcan1-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 82 Jan 17 22:20 zImage-imx6qp-sabreauto-gpmi-weim.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6qp-sabreauto-gpmi-weim-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 71 Jan 17 22:20 zImage-imx6q-sabreauto.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 77 Jan 17 22:20 zImage-imx6q-sabreauto-ecspi.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-ecspi-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 79 Jan 17 22:20 zImage-imx6q-sabreauto-enetirq.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-enetirq-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 80 Jan 17 22:20 zImage-imx6q-sabreauto-flexcan1.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-flexcan1-20190117131043.dtb
lrwxrwxrwx 2 kazmi kazmi 81 Jan 17 22:20 zImage-imx6q-sabreauto-gpmi-weim.dtb -> zImage--4.1-2.0.x+git0+6c1ad49339-r0-imx6q-sabreauto-gpmi-weim-20190117131043.dtb

My question is: If I want to manually transfer all the stuff to the SD card, where will I find the rootfs? Thanks

Regards,

Labels (3)
0 Kudos
Reply
2 Replies

1,287 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello,

Which BSP are you using? The BSP Release or the Community BSP?

Most newer BSPs or the newer branches use .ext4 which you should be able to use without problems to manually load the rootfs to your SD card.

In case it’s not being generated you can add this fs type on the IMAGE_FSTYPES variable, which can be setup on the conf/local.conf file inside your build directory.

IMAGE_FSTYPES = "ext3 tar.bz2"

I hope this helps!

Regards,

1,287 Views
husnain_kazmi
Contributor I

Hi gusarambula‌,

Thanks a lot for the reply. I added the fs type to the variable and it generated the rootfs with ext and tar.bz estensions. 

I am using the FSL Community BSP 

Can you please also help me out here: https://community.nxp.com/thread/493259 ?

Thanks in advance.

Regards,

Husnain

0 Kudos
Reply