Nitrogen6_max uboot from eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nitrogen6_max uboot from eMMC

1,172 Views
anandmistryk
Contributor II

Hi,

We are attempting to boot nitrogen6_max board from the eMMC.

It seems we'll have to program certain eFUSE since there is no boot-switch option.

Since these changes are irreversible, I wanted to know if it was safe to program the following fuses with following values? Are these changes sufficient to enable eMMC boot on nitrogen6_max board?

Before

BOOT_CFG[4:0]: 0x00000005: = 0x18000030

After

BOOT_CFG[4:0]: 0x00000005: = 0x18005878

Thanks and Regards,

Anand Mistry

Labels (1)
0 Kudos
Reply
0 Replies