New Android R10.3 BSP for i.MX50, i.MX51 and i.MX53 -blog archive
‎08-23-2011
01:48 PM
1,276 Views

EnriqueOchoaVaz
Contributor V
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The new Android R10.3 release is now available on the www.freescale.com page.
- Files available
Name | Description |
|
IMX5X_R10_3_ANDROID_DOCSBUNDLE | Android BSP Documentation. Includes Android R10.3 Release Notes and User's Guide |
IMX5X_R10_3_ANDROID_SOURCECODE | Android R10.3 Demo Image, documentation and Source Code for BSP and Codecs.. |
ACCP_CODECS_ANDROID_10_3 | ACC Plus Codec for Android R10.3 |
Target HW boards- i.MX50 EVK
- i.MX53 SABRE Tablet
- i.MX51 EVK
- What we got in this release:
- Base version is upgraded to android-2.3.4_rc1
- CTS 2.3_r4 (i.MX53 SABRE Tablet only)
- One time run.
- 13610 CTS case can be finished in one test cycle for most running.
- There is still possibility that CTS is stopped in following cases.
- USB cable need be reconnected: This is a known issue in CTS tool, which we have reported to Google.
- board freeze during reboot(<5%):Root cause still uncertain.
- Pass rate
- i.MX53 TABLET ---- 3 failure cases left among all 13610 cases
- 1 failure is caused by CTS case itself, which has been reported to Google CTS community.
- 2 failures are caused by the cellular network condition. These two cases are for 3G which failed to retrieve SMS delivery report within 5 minutes for fragmented long SMS.
- i.MX53 TABLET ---- 3 failure cases left among all 13610 cases
- Note: CTS result depends on many factors
- Tested Target (i.e. HW board, SW running on it)
The above pass rate (3 failure cases) is tested with specified test target (i.MX53 TABLET + Android R10.3 SW).
When running CTS on different target (e.g. on customer's board, or with modified SW), you may get various CTS result - Environment (i.e. cellular/wifi network condition, network configuration, HW board stability, etc)
Even with same test target (i.e. same HW+SW), run CTS several times may get various result. For example, those 2 3G related failures cases above may pass sometimes.
- Tested Target (i.e. HW board, SW running on it)
- Add some new features
- Enable android ringtone
- VPU firmware is upgraded to 1.4.41
- unlimited VPU instance number ( fix system slow down when long time flash playing)
- Enable HW BLT with Z160 on i.MX508, better performance when use LCD.
- Video playback on dual screen.
- Note: disabled in default ,please refer to user guide for enable it.
- Add back atheros ar6102 support in i.MX51
- Return to SD boot and ext4 file system as default on i.MX508
- Enable receive SMS and SMS deliver report for EM770W
- stability improvement
- 3G is more stable than before
- fix race condition issue (get wrong DNS for HuaWei 3G modem)
- fix DNS contamination between wifi and 3G.
- 3G is more stable than before
- One time run.
- What are the main issues left
- Storage
- UMS: In windows the SD card is full after erase, when the FAT partition is smaller than 64k cluster.
- Multimedia
- Camera: Picture of 5M pixel is not good.
- Power
- Battery status report of capacity is wrong
- Cannot resume from suspend after suspend/resume for 10+ times with camera preview
- connectivity
- OTG host<-->device function switch error
- BT PAIR/FTP between PC and device is unstable
- Storage
0 Replies