Negative temperature issue with IMX6D processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Negative temperature issue with IMX6D processor

1,219 次查看
Santhosha_rk
Contributor I

Hi,

We are running GPU test demo application supplied by freescale on our custom board having IMX6D processor. The test has been carried out at -20degC. The GPU application boots and application runs for some time, but image freezes after few seconds. The part selected has temperature range of -40 to 125degC. Please let us know what might be the problem.

-Santhosha RK

0 项奖励
回复
2 回复数

1,074 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Santhosha

this may be caused by ddr errors, so one can run ddr test on low temperatures

i.MX6/7 DDR Stress Test Tool V2.40

also recommended to check power supplies, as capacitors may work less

effectively at low temperatures and stability of 24MHz clock.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,074 次查看
Santhosha_rk
Contributor I

It was the problem with the implementation. supply voltage for core 2&3 were disabled in the schematics. While assembling supply input was connected to core 2 & 3 and the output was shorted. Processor was taking about 3W extra. When we removed the output side short, it worked at negative temperatures

0 项奖励
回复