Need to modify the "flash_headers.h" file from u-boot for DDR3 modification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need to modify the "flash_headers.h" file from u-boot for DDR3 modification

1,967 次查看
titusstalin
Contributor V

Dear All,

I'm newbie to iMX6 ARM processor. Sorry about silly question.

As I want to tweak the DDR3 registers for DDR3 leveling...

I want to change the RTT register in the flash header file ( MR1 register – 0x01C)

Also I would like to understand the meaning and effect of the identifier "i" of "MXC_DCD_ITEM" macro.

Can anyone help me to understand ?

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

1,671 次查看
igorpadykov
NXP Employee
NXP Employee

HI Titus

flash header is located in

ubootxx/board/freescale/mx6q_sabresd/flash_header.S

Identifier "i" of "MXC_DCD_ITEM" macro is used

for counting dcd header length

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,671 次查看
titusstalin
Contributor V

Hi,

Thanks for your quick reply.

I want to change the following registers.

ODT -> 0x818 (0x021B0818)

Output drive strength -> 0x800 (0x021B0800)

Processor part, write leveling -> 0x808 (0x021B0808)

DDR part, write leveling -> 0x01C (0x021B001c

I want to update these register in "flash_headers.S" file in u-boot with the following values.

ODT -> 0x818 (0x021B0818)  --> 0x0001111F

Output drive strength -> 0x800 (0x021B0800)  --> 0xA139556B

Processor part, write leveling -> 0x808 (0x021B0808)  --> 0x100

DDR part, write leveling -> 0x01C (0x021B001c  --> 0xC4

Can you please help to change the values in that file.

/*

* Copyright (C) 2012 Freescale Semiconductor, Inc.

*

* This program is free software; you can redistribute it and/or

* modify it under the terms of the GNU General Public License as

* published by the Free Software Foundation; either version 2 of

* the License, or (at your option) any later version.

*

* This program is distributed in the hope that it will be useful,

* but WITHOUT ANY WARRANTY; without even the implied warranty of

* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the

* GNU General Public License for more details.

*

* You should have received a copy of the GNU General Public License

* along with this program; if not, write to the Free Software

* Foundation, Inc., 59 Temple Place, Suite 330, Boston,

* MA 02111-1307 USA

*/

#include <config.h>

#include <asm/arch/mx6.h>

#ifdef    CONFIG_FLASH_HEADER

#ifndef CONFIG_FLASH_HEADER_OFFSET

# error "Must define the offset of flash header"

#endif

#define CPU_2_BE_32(l) \

       ((((l) & 0x000000FF) << 24) | \

    (((l) & 0x0000FF00) << 8)  | \

    (((l) & 0x00FF0000) >> 8)  | \

    (((l) & 0xFF000000) >> 24))

#define MXC_DCD_ITEM(i, addr, val)   \

dcd_node_##i:                        \

        .word CPU_2_BE_32(addr) ;     \

        .word CPU_2_BE_32(val)  ;     \

.section ".text.flasheader", "x"

    b    _start

    .org    CONFIG_FLASH_HEADER_OFFSET

ivt_header:       .word 0x402000D1 /* Tag=0xD1, Len=0x0020, Ver=0x40 */

app_code_jump_v:  .word _start

reserv1:          .word 0x0

dcd_ptr:          .word dcd_hdr

boot_data_ptr:      .word boot_data

self_ptr:         .word ivt_header

#ifdef CONFIG_SECURE_BOOT

app_code_csf:     .word __hab_data

#else

app_code_csf:     .word 0x0

#endif

reserv2:          .word 0x0

boot_data:        .word TEXT_BASE

#ifdef CONFIG_SECURE_BOOT

image_len:        .word __hab_data_end - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET

#else

image_len:        .word _end_of_copy  - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET

#endif

plugin:           .word 0x0

#if defined CONFIG_MX6DL_DDR3

#if defined CONFIG_DDR_32BIT

dcd_hdr:          .word 0x40E001D2 /* Tag=0xD2, Len=59*8 + 4 + 4, Ver=0x40 */

write_dcd_cmd:    .word 0x04DC01CC /* Tag=0xCC, Len=59*8 + 4, Param=0x04 */

MXC_DCD_ITEM(1, IOMUXC_BASE_ADDR + 0x774, 0x000C0000)

MXC_DCD_ITEM(2, IOMUXC_BASE_ADDR + 0x754, 0x00000000)

MXC_DCD_ITEM(3, IOMUXC_BASE_ADDR + 0x4ac, 0x00000030)

MXC_DCD_ITEM(4, IOMUXC_BASE_ADDR + 0x4b0, 0x00000030)

MXC_DCD_ITEM(5, IOMUXC_BASE_ADDR + 0x464, 0x00000030)

MXC_DCD_ITEM(6, IOMUXC_BASE_ADDR + 0x490, 0x00000030)

MXC_DCD_ITEM(7, IOMUXC_BASE_ADDR + 0x74c, 0x00000030)

MXC_DCD_ITEM(8, IOMUXC_BASE_ADDR + 0x494, 0x00000030)

MXC_DCD_ITEM(9, IOMUXC_BASE_ADDR + 0x4a0, 0x00000000)

MXC_DCD_ITEM(10, IOMUXC_BASE_ADDR + 0x4b4, 0x00000030)

MXC_DCD_ITEM(11, IOMUXC_BASE_ADDR + 0x4b8, 0x00000030)

MXC_DCD_ITEM(12, IOMUXC_BASE_ADDR + 0x76c, 0x00000030)

MXC_DCD_ITEM(13, IOMUXC_BASE_ADDR + 0x750, 0x00020000)

MXC_DCD_ITEM(14, IOMUXC_BASE_ADDR + 0x4bc, 0x00000030)

MXC_DCD_ITEM(15, IOMUXC_BASE_ADDR + 0x4c0, 0x00000030)

MXC_DCD_ITEM(16, IOMUXC_BASE_ADDR + 0x4c4, 0x00000030)

MXC_DCD_ITEM(17, IOMUXC_BASE_ADDR + 0x4c8, 0x00000030)

MXC_DCD_ITEM(18, IOMUXC_BASE_ADDR + 0x760, 0x00020000)

MXC_DCD_ITEM(19, IOMUXC_BASE_ADDR + 0x764, 0x00000030)

MXC_DCD_ITEM(20, IOMUXC_BASE_ADDR + 0x770, 0x00000030)

MXC_DCD_ITEM(21, IOMUXC_BASE_ADDR + 0x778, 0x00000030)

MXC_DCD_ITEM(22, IOMUXC_BASE_ADDR + 0x77c, 0x00000030)

MXC_DCD_ITEM(23, IOMUXC_BASE_ADDR + 0x470, 0x00000030)

MXC_DCD_ITEM(24, IOMUXC_BASE_ADDR + 0x474, 0x00000030)

MXC_DCD_ITEM(25, IOMUXC_BASE_ADDR + 0x478, 0x00000030)

MXC_DCD_ITEM(26, IOMUXC_BASE_ADDR + 0x47c, 0x00000030)

MXC_DCD_ITEM(27, MMDC_P0_BASE_ADDR + 0x800, 0xA1390003)

MXC_DCD_ITEM(28, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)

MXC_DCD_ITEM(29, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)

MXC_DCD_ITEM(30, MMDC_P0_BASE_ADDR + 0x83c, 0x42190219)

MXC_DCD_ITEM(31, MMDC_P0_BASE_ADDR + 0x840, 0x017B0177)

MXC_DCD_ITEM(32, MMDC_P0_BASE_ADDR + 0x848, 0x4B4D4E4D)

MXC_DCD_ITEM(33, MMDC_P0_BASE_ADDR + 0x850, 0x3F3E2D36)

MXC_DCD_ITEM(34, MMDC_P0_BASE_ADDR + 0x81c, 0x33333333)

MXC_DCD_ITEM(35, MMDC_P0_BASE_ADDR + 0x820, 0x33333333)

MXC_DCD_ITEM(36, MMDC_P0_BASE_ADDR + 0x824, 0x33333333)

MXC_DCD_ITEM(37, MMDC_P0_BASE_ADDR + 0x828, 0x33333333)

MXC_DCD_ITEM(38, MMDC_P0_BASE_ADDR + 0x8b8, 0x00000800)

MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x004, 0x0002002D)

MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x008, 0x00333030)

MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x00c, 0x3F435313)

MXC_DCD_ITEM(42, MMDC_P0_BASE_ADDR + 0x010, 0xB66E8B63)

MXC_DCD_ITEM(43, MMDC_P0_BASE_ADDR + 0x014, 0x01FF00DB)

MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x018, 0x00001740)

MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x01c, 0x00008000)

MXC_DCD_ITEM(46, MMDC_P0_BASE_ADDR + 0x02c, 0x000026d2)

MXC_DCD_ITEM(47, MMDC_P0_BASE_ADDR + 0x030, 0x00431023)

MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x040, 0x00000017)

MXC_DCD_ITEM(49, MMDC_P0_BASE_ADDR + 0x000, 0x83190000)

MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x01c, 0x04008032)

MXC_DCD_ITEM(51, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)

MXC_DCD_ITEM(52, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)

MXC_DCD_ITEM(53, MMDC_P0_BASE_ADDR + 0x01c, 0x05208030)

MXC_DCD_ITEM(54, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)

MXC_DCD_ITEM(55, MMDC_P0_BASE_ADDR + 0x020, 0x00005800)

MXC_DCD_ITEM(56, MMDC_P0_BASE_ADDR + 0x818, 0x00011117)

MXC_DCD_ITEM(57, MMDC_P0_BASE_ADDR + 0x004, 0x0002556d)

MXC_DCD_ITEM(58, MMDC_P0_BASE_ADDR + 0x404, 0x00011006)

MXC_DCD_ITEM(59, MMDC_P0_BASE_ADDR + 0x01c, 0x00000000)

#else /* i.MX6DL 64BIT-DDR */

dcd_hdr:          .word 0x40A002D2 /* Tag=0xD2, Len=83*8 + 4 + 4, Ver=0x40 */

write_dcd_cmd:    .word 0x049C02CC /* Tag=0xCC, Len=83*8 + 4, Param=0x04 */

# IOMUXC_BASE_ADDR  = 0x20e0000

# DDR IO TYPE

MXC_DCD_ITEM(1, IOMUXC_BASE_ADDR + 0x774, 0x000c0000)

MXC_DCD_ITEM(2, IOMUXC_BASE_ADDR + 0x754, 0x00000000)

# Clock

MXC_DCD_ITEM(3, IOMUXC_BASE_ADDR + 0x4ac, 0x00000030)

MXC_DCD_ITEM(4, IOMUXC_BASE_ADDR + 0x4b0, 0x00000030)

# Address

MXC_DCD_ITEM(5, IOMUXC_BASE_ADDR + 0x464, 0x00000030)

MXC_DCD_ITEM(6, IOMUXC_BASE_ADDR + 0x490, 0x00000030)

MXC_DCD_ITEM(7, IOMUXC_BASE_ADDR + 0x74c, 0x00000030)

# Control

MXC_DCD_ITEM(8, IOMUXC_BASE_ADDR + 0x494, 0x00000030)

MXC_DCD_ITEM(9, IOMUXC_BASE_ADDR + 0x4a0, 0x00000000)

MXC_DCD_ITEM(10, IOMUXC_BASE_ADDR + 0x4b4, 0x00000030)

MXC_DCD_ITEM(11, IOMUXC_BASE_ADDR + 0x4b8, 0x00000030)

MXC_DCD_ITEM(12, IOMUXC_BASE_ADDR + 0x76c, 0x00000030)

# Data Strobe

MXC_DCD_ITEM(13, IOMUXC_BASE_ADDR + 0x750, 0x00020000)

MXC_DCD_ITEM(14, IOMUXC_BASE_ADDR + 0x4bc, 0x00000030)

MXC_DCD_ITEM(15, IOMUXC_BASE_ADDR + 0x4c0, 0x00000030)

MXC_DCD_ITEM(16, IOMUXC_BASE_ADDR + 0x4c4, 0x00000030)

MXC_DCD_ITEM(17, IOMUXC_BASE_ADDR + 0x4c8, 0x00000030)

MXC_DCD_ITEM(18, IOMUXC_BASE_ADDR + 0x4cc, 0x00000030)

MXC_DCD_ITEM(19, IOMUXC_BASE_ADDR + 0x4d0, 0x00000030)

MXC_DCD_ITEM(20, IOMUXC_BASE_ADDR + 0x4d4, 0x00000030)

MXC_DCD_ITEM(21, IOMUXC_BASE_ADDR + 0x4d8, 0x00000030)

MXC_DCD_ITEM(22, IOMUXC_BASE_ADDR + 0x760, 0x00020000)

MXC_DCD_ITEM(23, IOMUXC_BASE_ADDR + 0x764, 0x00000030)

MXC_DCD_ITEM(24, IOMUXC_BASE_ADDR + 0x770, 0x00000030)

MXC_DCD_ITEM(25, IOMUXC_BASE_ADDR + 0x778, 0x00000030)

MXC_DCD_ITEM(26, IOMUXC_BASE_ADDR + 0x77c, 0x00000030)

MXC_DCD_ITEM(27, IOMUXC_BASE_ADDR + 0x780, 0x00000030)

MXC_DCD_ITEM(28, IOMUXC_BASE_ADDR + 0x784, 0x00000030)

MXC_DCD_ITEM(29, IOMUXC_BASE_ADDR + 0x78c, 0x00000030)

MXC_DCD_ITEM(30, IOMUXC_BASE_ADDR + 0x748, 0x00000030)

MXC_DCD_ITEM(31, IOMUXC_BASE_ADDR + 0x470, 0x00000030)

MXC_DCD_ITEM(32, IOMUXC_BASE_ADDR + 0x474, 0x00000030)

MXC_DCD_ITEM(33, IOMUXC_BASE_ADDR + 0x478, 0x00000030)

MXC_DCD_ITEM(34, IOMUXC_BASE_ADDR + 0x47c, 0x00000030)

MXC_DCD_ITEM(35, IOMUXC_BASE_ADDR + 0x480, 0x00000030)

MXC_DCD_ITEM(36, IOMUXC_BASE_ADDR + 0x484, 0x00000030)

MXC_DCD_ITEM(37, IOMUXC_BASE_ADDR + 0x488, 0x00000030)

MXC_DCD_ITEM(38, IOMUXC_BASE_ADDR + 0x48c, 0x00000030)

# MMDC_P0_BASE_ADDR = 0x021b0000

# MMDC_P1_BASE_ADDR = 0x021b4000

# Calibrations

# ZQ

MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x800, 0xa1390003)

# write leveling

MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)

MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)

MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)

MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)

# DQS gating, read delay, write delay calibration values

# based on calibration compare of 0x00ffff00

MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x83c, 0x42480248)

MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x840, 0x0211020B)

MXC_DCD_ITEM(46, MMDC_P1_BASE_ADDR + 0x83C, 0x417F0211)

MXC_DCD_ITEM(47, MMDC_P1_BASE_ADDR + 0x840, 0x015D0166)

MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x848, 0x4B4C504D)

MXC_DCD_ITEM(49, MMDC_P1_BASE_ADDR + 0x848, 0x494C4F48)

MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x850, 0x3F3F2E31)

MXC_DCD_ITEM(51, MMDC_P1_BASE_ADDR + 0x850, 0x2B35382B)

MXC_DCD_ITEM(52, MMDC_P0_BASE_ADDR + 0x81c, 0x33333333)

MXC_DCD_ITEM(53, MMDC_P0_BASE_ADDR + 0x820, 0x33333333)

MXC_DCD_ITEM(54, MMDC_P0_BASE_ADDR + 0x824, 0x33333333)

MXC_DCD_ITEM(55, MMDC_P0_BASE_ADDR + 0x828, 0x33333333)

MXC_DCD_ITEM(56, MMDC_P1_BASE_ADDR + 0x81c, 0x33333333)

MXC_DCD_ITEM(57, MMDC_P1_BASE_ADDR + 0x820, 0x33333333)

MXC_DCD_ITEM(58, MMDC_P1_BASE_ADDR + 0x824, 0x33333333)

MXC_DCD_ITEM(59, MMDC_P1_BASE_ADDR + 0x828, 0x33333333)

MXC_DCD_ITEM(60, MMDC_P0_BASE_ADDR + 0x8b8, 0x00000800)

MXC_DCD_ITEM(61, MMDC_P1_BASE_ADDR + 0x8b8, 0x00000800)

# MMDC init:

# in DDR3, 64-bit mode, only MMDC0 is initiated:

MXC_DCD_ITEM(62, MMDC_P0_BASE_ADDR + 0x004, 0x0002002D)

MXC_DCD_ITEM(63, MMDC_P0_BASE_ADDR + 0x008, 0x00333030)

MXC_DCD_ITEM(64, MMDC_P0_BASE_ADDR + 0x00c, 0x3F435313)

MXC_DCD_ITEM(65, MMDC_P0_BASE_ADDR + 0x010, 0xB66E8B63)

MXC_DCD_ITEM(66, MMDC_P0_BASE_ADDR + 0x014, 0x01FF00DB)

MXC_DCD_ITEM(67, MMDC_P0_BASE_ADDR + 0x018, 0x00081740)

MXC_DCD_ITEM(68, MMDC_P0_BASE_ADDR + 0x01c, 0x00008000)

MXC_DCD_ITEM(69, MMDC_P0_BASE_ADDR + 0x02c, 0x000026d2)

MXC_DCD_ITEM(70, MMDC_P0_BASE_ADDR + 0x030, 0x00431023)

MXC_DCD_ITEM(71, MMDC_P0_BASE_ADDR + 0x040, 0x00000027)

MXC_DCD_ITEM(72, MMDC_P0_BASE_ADDR + 0x000, 0x831A0000)

# Initialize 2GB DDR3 - Micron MT41J128M

MXC_DCD_ITEM(73, MMDC_P0_BASE_ADDR + 0x01c, 0x04008032)

MXC_DCD_ITEM(74, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)

MXC_DCD_ITEM(75, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)

MXC_DCD_ITEM(76, MMDC_P0_BASE_ADDR + 0x01c, 0x05208030)

MXC_DCD_ITEM(77, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)

MXC_DCD_ITEM(78, MMDC_P0_BASE_ADDR + 0x020, 0x00005800)

MXC_DCD_ITEM(79, MMDC_P0_BASE_ADDR + 0x818, 0x00011117)

MXC_DCD_ITEM(80, MMDC_P1_BASE_ADDR + 0x818, 0x00011117)

MXC_DCD_ITEM(81, MMDC_P0_BASE_ADDR + 0x004, 0x0002556d)

MXC_DCD_ITEM(82, MMDC_P1_BASE_ADDR + 0x404, 0x00011006)

MXC_DCD_ITEM(83, MMDC_P0_BASE_ADDR + 0x01c, 0x00000000)

#endif

#else  /* i.MX6Q */

dcd_hdr:          .word 0x40a002D2 /* Tag=0xD2, Len=83*8 + 4 + 4, Ver=0x40 */

write_dcd_cmd:    .word 0x049c02CC /* Tag=0xCC, Len=83*8 + 4, Param=0x04 */

/* DCD */

MXC_DCD_ITEM(1, IOMUXC_BASE_ADDR + 0x798, 0x000C0000)

MXC_DCD_ITEM(2, IOMUXC_BASE_ADDR + 0x758, 0x00000000)

MXC_DCD_ITEM(3, IOMUXC_BASE_ADDR + 0x588, 0x00000030)

MXC_DCD_ITEM(4, IOMUXC_BASE_ADDR + 0x594, 0x00000030)

MXC_DCD_ITEM(5, IOMUXC_BASE_ADDR + 0x56c, 0x00000030)

MXC_DCD_ITEM(6, IOMUXC_BASE_ADDR + 0x578, 0x00000030)

MXC_DCD_ITEM(7, IOMUXC_BASE_ADDR + 0x74c, 0x00000030)

MXC_DCD_ITEM(8, IOMUXC_BASE_ADDR + 0x57c, 0x00000030)

MXC_DCD_ITEM(9, IOMUXC_BASE_ADDR + 0x58c, 0x00000000)

MXC_DCD_ITEM(10, IOMUXC_BASE_ADDR + 0x59c, 0x00000030)

MXC_DCD_ITEM(11, IOMUXC_BASE_ADDR + 0x5a0, 0x00000030)

MXC_DCD_ITEM(12, IOMUXC_BASE_ADDR + 0x78c, 0x00000030)

MXC_DCD_ITEM(13, IOMUXC_BASE_ADDR + 0x750, 0x00020000)

MXC_DCD_ITEM(14, IOMUXC_BASE_ADDR + 0x5a8, 0x00000030)

MXC_DCD_ITEM(15, IOMUXC_BASE_ADDR + 0x5b0, 0x00000030)

MXC_DCD_ITEM(16, IOMUXC_BASE_ADDR + 0x524, 0x00000030)

MXC_DCD_ITEM(17, IOMUXC_BASE_ADDR + 0x51c, 0x00000030)

MXC_DCD_ITEM(18, IOMUXC_BASE_ADDR + 0x518, 0x00000030)

MXC_DCD_ITEM(19, IOMUXC_BASE_ADDR + 0x50c, 0x00000030)

MXC_DCD_ITEM(20, IOMUXC_BASE_ADDR + 0x5b8, 0x00000030)

MXC_DCD_ITEM(21, IOMUXC_BASE_ADDR + 0x5c0, 0x00000030)

MXC_DCD_ITEM(22, IOMUXC_BASE_ADDR + 0x774, 0x00020000)

MXC_DCD_ITEM(23, IOMUXC_BASE_ADDR + 0x784, 0x00000030)

MXC_DCD_ITEM(24, IOMUXC_BASE_ADDR + 0x788, 0x00000030)

MXC_DCD_ITEM(25, IOMUXC_BASE_ADDR + 0x794, 0x00000030)

MXC_DCD_ITEM(26, IOMUXC_BASE_ADDR + 0x79c, 0x00000030)

MXC_DCD_ITEM(27, IOMUXC_BASE_ADDR + 0x7a0, 0x00000030)

MXC_DCD_ITEM(28, IOMUXC_BASE_ADDR + 0x7a4, 0x00000030)

MXC_DCD_ITEM(29, IOMUXC_BASE_ADDR + 0x7a8, 0x00000030)

MXC_DCD_ITEM(30, IOMUXC_BASE_ADDR + 0x748, 0x00000030)

MXC_DCD_ITEM(31, IOMUXC_BASE_ADDR + 0x5ac, 0x00000030)

MXC_DCD_ITEM(32, IOMUXC_BASE_ADDR + 0x5b4, 0x00000030)

MXC_DCD_ITEM(33, IOMUXC_BASE_ADDR + 0x528, 0x00000030)

MXC_DCD_ITEM(34, IOMUXC_BASE_ADDR + 0x520, 0x00000030)

MXC_DCD_ITEM(35, IOMUXC_BASE_ADDR + 0x514, 0x00000030)

MXC_DCD_ITEM(36, IOMUXC_BASE_ADDR + 0x510, 0x00000030)

MXC_DCD_ITEM(37, IOMUXC_BASE_ADDR + 0x5bc, 0x00000030)

MXC_DCD_ITEM(38, IOMUXC_BASE_ADDR + 0x5c4, 0x00000030)

MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x800, 0xA1390003)

MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)

MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)

MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)

MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)

MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x83c, 0x4333033F)

MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x840, 0x032C031D)

MXC_DCD_ITEM(46, MMDC_P1_BASE_ADDR + 0x83c, 0x43200332)

MXC_DCD_ITEM(47, MMDC_P1_BASE_ADDR + 0x840, 0x031A026A)

MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x848, 0x4D464746)

MXC_DCD_ITEM(49, MMDC_P1_BASE_ADDR + 0x848, 0x47453F4D)

MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x850, 0x3E434440)

MXC_DCD_ITEM(51, MMDC_P1_BASE_ADDR + 0x850, 0x47384839)

MXC_DCD_ITEM(52, MMDC_P0_BASE_ADDR + 0x81c, 0x33333333)

MXC_DCD_ITEM(53, MMDC_P0_BASE_ADDR + 0x820, 0x33333333)

MXC_DCD_ITEM(54, MMDC_P0_BASE_ADDR + 0x824, 0x33333333)

MXC_DCD_ITEM(55, MMDC_P0_BASE_ADDR + 0x828, 0x33333333)

MXC_DCD_ITEM(56, MMDC_P1_BASE_ADDR + 0x81c, 0x33333333)

MXC_DCD_ITEM(57, MMDC_P1_BASE_ADDR + 0x820, 0x33333333)

MXC_DCD_ITEM(58, MMDC_P1_BASE_ADDR + 0x824, 0x33333333)

MXC_DCD_ITEM(59, MMDC_P1_BASE_ADDR + 0x828, 0x33333333)

MXC_DCD_ITEM(60, MMDC_P0_BASE_ADDR + 0x8b8, 0x00000800)

MXC_DCD_ITEM(61, MMDC_P1_BASE_ADDR + 0x8b8, 0x00000800)

MXC_DCD_ITEM(62, MMDC_P0_BASE_ADDR + 0x004, 0x00020036)

MXC_DCD_ITEM(63, MMDC_P0_BASE_ADDR + 0x008, 0x09444040)

MXC_DCD_ITEM(64, MMDC_P0_BASE_ADDR + 0x00c, 0x555A7975)

MXC_DCD_ITEM(65, MMDC_P0_BASE_ADDR + 0x010, 0xFF538F64)

MXC_DCD_ITEM(66, MMDC_P0_BASE_ADDR + 0x014, 0x01FF00DB)

MXC_DCD_ITEM(67, MMDC_P0_BASE_ADDR + 0x018, 0x00001740)

MXC_DCD_ITEM(68, MMDC_P0_BASE_ADDR + 0x01c, 0x00008000)

MXC_DCD_ITEM(69, MMDC_P0_BASE_ADDR + 0x02c, 0x000026D2)

MXC_DCD_ITEM(70, MMDC_P0_BASE_ADDR + 0x030, 0x005A1023)

MXC_DCD_ITEM(71, MMDC_P0_BASE_ADDR + 0x040, 0x00000027)

MXC_DCD_ITEM(72, MMDC_P0_BASE_ADDR + 0x000, 0x831A0000)

MXC_DCD_ITEM(73, MMDC_P0_BASE_ADDR + 0x01c, 0x04088032)

MXC_DCD_ITEM(74, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)

MXC_DCD_ITEM(75, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)

MXC_DCD_ITEM(76, MMDC_P0_BASE_ADDR + 0x01c, 0x09408030)

MXC_DCD_ITEM(77, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)

MXC_DCD_ITEM(78, MMDC_P0_BASE_ADDR + 0x020, 0x00005800)

MXC_DCD_ITEM(79, MMDC_P0_BASE_ADDR + 0x818, 0x00011117)

MXC_DCD_ITEM(80, MMDC_P1_BASE_ADDR + 0x818, 0x00011117)

MXC_DCD_ITEM(81, MMDC_P0_BASE_ADDR + 0x004, 0x00025576)

MXC_DCD_ITEM(82, MMDC_P0_BASE_ADDR + 0x404, 0x00011006)

MXC_DCD_ITEM(83, MMDC_P0_BASE_ADDR + 0x01c, 0x00000000)

#endif

#endif

0 项奖励
回复

1,671 次查看
igorpadykov
NXP Employee
NXP Employee

please find attached file flash_header.S

change it or add lines for example for write leveling:

"# write leveling

MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F) "

~igor

1,671 次查看
titusstalin
Contributor V

Why do we have the following different values for the same address with different "i" identifier value ?

MXC_DCD_ITEM(73, MMDC_P0_BASE_ADDR + 0x01c, 0x04088032)

MXC_DCD_ITEM(74, MMDC_P0_BASE_ADDR + 0x01c, 0x00008033)

MXC_DCD_ITEM(75, MMDC_P0_BASE_ADDR + 0x01c, 0x00048031)

MXC_DCD_ITEM(76, MMDC_P0_BASE_ADDR + 0x01c, 0x09408030)

MXC_DCD_ITEM(77, MMDC_P0_BASE_ADDR + 0x01c, 0x04008040)

change it or add lines for example for write leveling:

"# write leveling

MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F) "

Where I need to add the above line ? anywhere ? or last line of the *.S file ?

Also, that line is already available right !

Why we are using particularly "40" ?

Any "i" identifier value we can use ?

MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)

MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)

MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)

MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)

please find attached file flash_header.S

Did you change anything in this attached file ?

I'm newbie to this, sorry for the very basic questions.

Thanks for your support.

0 项奖励
回复