Need to interface 13MP camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need to interface 13MP camera

1,519件の閲覧回数
titusstalin
Contributor V

Hello Experts,

I need to interface the 13MP camera to imx6 dual/quad processor.

The output format should be RGB or YUV but not RAW/bayer format as imx's IPU doesn't support conversion from RAW to any format on the fly, need SW effort.

The camera can be MIPI or serial or parallel, any sensor interface which suits to imx6.

Regards,

Titus S.

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,348件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you want to know tested 13MP camera part numberr for mx6Q? i f yes, I found other customer try to use e-CAM130_CUMI1820_MOD - 13 MP Camera module based on Aptina’s AR1820HS sensor , but they tested on the third-party board, for mx6Q, we don't have tested 13MP camera

0 件の賞賛
返信