Need the source code of 'tvsrc' (libmfw_gst_tvsrc.so)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need the source code of 'tvsrc' (libmfw_gst_tvsrc.so)

ソリューションへジャンプ
2,723件の閲覧回数
RobbieJiang
Contributor IV

Hi,

Currently the 'tvsrc' element works with my CSI camera on MX6Q/Linux platform.

However, we would like to make some changes to 'tvsrc', e.g, to add some new attributes,

or to support more input resolutions.

So the source code of 'tvsrc' is needed.

But I have only the binary code of libmfw_gst_tvsrc.so,

where can I get the source code?

Regards,

Jie

ラベル(3)
1 解決策
2,470件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

in gst-fsl-plugins-3.0.11.tar.gz I found

1.jpg

2.jpg

~igor

元の投稿で解決策を見る

4 返答(返信)
2,470件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

had you looked in gst-fsl-plugins L3.0.35_4.1.0_MM_CODECS

Middleware-Codecs and other Algorithms (11)

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

0 件の賞賛
返信
2,470件の閲覧回数
RobbieJiang
Contributor IV

Hi igor,

In the codecs packaged you mentioned,

there is no source code for tvsrc.

Is it a third party software?

Why is fsl's 'mfw_v4lsrc'  not used and replaced by tvsrc?

Regards,

Robbie

0 件の賞賛
返信
2,471件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

in gst-fsl-plugins-3.0.11.tar.gz I found

1.jpg

2.jpg

~igor

2,470件の閲覧回数
RobbieJiang
Contributor IV

Hi igor,

Thanks for your information.

I tried to download  L3.0.35_4.1.0_MM_CODECS,

but actually it is included in L3.0.101_4.1.1_MM_CODECS.

Anyway,  thanks a lot!

Regards,

Jie

0 件の賞賛
返信