Need the OS to boot using the quad SPI, in one case, and using USDHC-1 4-bit, in the other, how do I need to configure the boot_mode conclusions (5: 0) to do this?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need the OS to boot using the quad SPI, in one case, and using USDHC-1 4-bit, in the other, how do I need to configure the boot_mode conclusions (5: 0) to do this?

764件の閲覧回数
sasha_yakovlev9
Contributor I

I am developing a module based on processor i.MX8 Quad Max.
I need the OS to boot using the quad SPI, in one case, and using USDHC-1 4-bit, in the other, how do I need to configure the boot_mode conclusions (5: 0) to do this?


I didn't find any information about this in the "i.MX 8QuadMax Automotive and Infotainment Applications Processors" or in the "i.MX8 QM / i.MX8 QXP Hardware Developer’s Guide". "I.MX 8QuadMax Automotive and Infotainment Applications Processors" refers to the "reference manual", but I didn't find it for this processor. The configuration for loading the octal SPI is indicated in the pdf file of the EVK board circuit, but this isn't what I need.
I would appreciate it if you tell me where I can find this information on setting up the boot configuration for this processor.

With appreciation, Alexander

ラベル(1)
0 件の賞賛
返信
0 返答(返信)