Need some advice with SOF Integration(Resources)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need some advice with SOF Integration(Resources)

1,071 次查看
hasnain_akhtar
Contributor I

Hi there!

Complete newbie here. I just wanted to ask if SOF is already built in the board? I can access the aplay and amixer parameters within the board(via simple serial connection). I am trying to build an SOF environment in a Linux OS since the sof would be a more updated version. Trying to add additional audio modules to be integrated in the board. Any other resources available besides the SOF website? Thanks!

2 回复数

1,033 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hasnain

I am afraid it is not integrated, Linux  documentation Linux 5.4.3_1.0.0 Documentation
i.MX Software | NXP 

describes what is integrated in nxp bsps.

One can try to follow Porting Guide included in linux documentation and

Build SOF from scratch — SOF Project 0.1 documentation 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,033 次查看
hasnain_akhtar
Contributor I

I have been following the same porting guide from SOF. But nevertheless thank you for your response!

0 项奖励
回复