Nand flash not getting detected in iMX6X processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Nand flash not getting detected in iMX6X processor

跳至解决方案
3,516 次查看
Sowmya1z
Contributor II

Dear all,

  I am porting Nand flash driver in iMX6X WinCE 7.0 platform. I am using micron's MT29F4G16ABBDAHC nand. nand is not detecting in wince 7.0. once the wince OS is launched i am getting "No NAND type matched" print in the hyper terminal.

i added the following entries for supporting the "MT29F4G16ABBDAHC" nand in the NANDTYPES.h file:

{
        {NAND, 4096, 2048 * 64, 64, 2048},  //spare area bytes are not considered       
        {0x2C, 0xBC, 0x90, 0x55},                   //BYTE        NANDCode[NANDID_LENGTH]
        3,                                          //BYTE        NumBlockCycles
        5,                                          //BYTE        ChipAddrCycleNum
        16,                                          //BYTE        DataWidth
        1,                                          //BYTE        BBMarkNum
        {0},                                        //BYTE        BBMarkPage
        6,                                          //BYTE        StatusBusyBit
        0,                                          //BYTE        StatusErrorBit
        64,                                         //WORD        SpareDataLength
        0x70,                                       //BYTE        CmdReadStatus
        0x00,                                       //BYTE        CmdRead1
        0x30,                                       //BYTE        CmdRead2
        0x90,                                       //BYTE        CmdReadId
        0xff,                                       //BYTE        CmdReset
        0x80,                                       //BYTE        CmdWrite1
        0x10,                                       //BYTE        CmdWrite2
        0x60,                                       //BYTE        CmdErase1
        0xD0,                                       //BYTE        CmdErase2
        {25, 16, 25, 20}                             //NANDTiming  timings

}
     The driver is returning the nand id as 0.  I configured the GPMICLK to 198MHz, AHB clock to 132MHz.

 Please help me to solve this issue.

Regards,

Sowmya

标签 (1)
0 项奖励
回复
1 解答
1,704 次查看
VladanJovanovic
NXP Employee
NXP Employee

This is obviously SW issue that is difficult to answer here as WinCE7 comes from 3rd party.

Few easy steps to check:

- do you see any activity on NAND bus pins?

- does the driver start to communicate succesfully with the NAND (read ID etc., basic init )

- are clocks to NAND controller enabled?

- are pins set up for NAND operation (no other SW module is reconfiguring IOMUX for other operation)?

this should get you started finding the root cause of problem.

Vladan

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,705 次查看
VladanJovanovic
NXP Employee
NXP Employee

This is obviously SW issue that is difficult to answer here as WinCE7 comes from 3rd party.

Few easy steps to check:

- do you see any activity on NAND bus pins?

- does the driver start to communicate succesfully with the NAND (read ID etc., basic init )

- are clocks to NAND controller enabled?

- are pins set up for NAND operation (no other SW module is reconfiguring IOMUX for other operation)?

this should get you started finding the root cause of problem.

Vladan

0 项奖励
回复
1,704 次查看
Sowmya1z
Contributor II

Dear Vladan,

Thank you for the reply.The APBH is not initialized. After initializing the APBH channel, NAND is detected. Now iam able to read and write to the NAND.

Regards,

Sowmya

0 项奖励
回复