NXP i.MX Release Distro OS is slow in executing commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP i.MX Release Distro OS is slow in executing commands

1,679件の閲覧回数
rajspatel1297
Contributor I

I'm using imx7 with NXP i.MX Release Distro 5.10-hardknott (hardknott).

It is very slow in executing commands such as node and npm. 

I checked with Debian 10 but it's working fine in that. 

So is there any additional tuning requirement for that?

 

Operating System: NXP i.MX Release Distro 5.10-hardknott (hardknott)
Kernel: Linux 5.10.9
Architecture: arm

ID=fsl-imx-xwayland
NAME="NXP i.MX Release Distro"
VERSION="5.10-hardknott (hardknott)"
VERSION_ID=5.10-hardknott
PRETTY_NAME="NXP i.MX Release Distro 5.10-hardknott (hardknott)"

 

ラベル(2)
0 件の賞賛
返信
1 返信

1,660件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rajspatel,

You migth try the L.510.52 BSP that have a lot of kernel enhancement and bug fixed from prevously kernels.

https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Regards

0 件の賞賛
返信