NXP eIQ ML Enablement Yocto build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP eIQ ML Enablement Yocto build error

ソリューションへジャンプ
4,410件の閲覧回数
davidvescovi
Contributor V

I have been following https://www.nxp.com/docs/en/nxp/user-guides/UM11226.pdf  and building with Yocto but I am getting several gstreamer do_fetch errors for example:

NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: gstreamer1.0-1.14.4.imx-r0 do_fetch: Failed to fetch URL gitsm://source.codeaurora.org/external/imx/gstreamer.git;protocol=https;branch=MM_04.04.05_1902_L4.14.98_GA, attempting MIRRORS if available
ERROR: gstreamer1.0-1.14.4.imx-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export PATH="/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0/1.14.4.imx-r0/recipe-sysroot-native/usr/bin/python3-native:/datadrive/imx_yocto-bspml/sources/poky/scripts:/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0/1.14.4.imx-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0/1.14.4.imx-r0/recipe-sysroot/usr/bin/crossscripts:/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0/1.14.4.imx-r0/recipe-sysroot-native/usr/sbin:/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0/1.14.4.imx-r0/recipe-sysroot-native/usr/bin:/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0/1.14.4.imx-r0/recipe-sysroot-native/sbin:/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0/1.14.4.imx-r0/recipe-sysroot-native/bin:/datadrive/imx_yocto-bspml/sources/poky/bitbake/bin:/datadrive/imx_yocto-bspml/bld8qm_xwayland/tmp/hosttools"; export HOME="/home/david"; git -c core.fsyncobjectfiles=0 submodule update --init --recursive failed with exit code 1, output:...

Does anyone no how to correct the recipe? It looks like it might not be the latest or the URL is wrong?

ラベル(1)
0 件の賞賛
返信
1 解決策
4,189件の閲覧回数
davidvescovi
Contributor V

seems to have mysteriously healed itself … must have been a network or server error.

I did not change anything. 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,189件の閲覧回数
danwei_luo
NXP Employee
NXP Employee

I met the same issue while compiling on Jun 3, I will try it today to check whether it's healed.

Thanks, David.

Best regards,

Danwei

0 件の賞賛
返信
3,224件の閲覧回数
farooq
Contributor II
I am facing the same problem now.
ERROR: gstreamer1.0-1.14.imx-r0 do_fetch: Fetcher failure for URL: 'gitsm://source.codeaurora.org/external/imx/gstreamer.git;protocol=https;branch=MM_04.04.02_1808_L4.9.123_MX8MM_GA'. Unable to fetch URL from any source.

Do you really think it is a network issue ?

0 件の賞賛
返信
4,190件の閲覧回数
davidvescovi
Contributor V

seems to have mysteriously healed itself … must have been a network or server error.

I did not change anything. 

0 件の賞賛
返信