NXP and display timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP and display timing

918 Views
mspenard603
Contributor IV

I’ve been a bit confused on how display timing is documented. It seems inconsistent to myself. And, so, I was hoping you could clarify if there really is a discrepancy in my understanding or in the docs. As the NXP SDK seems to be looking for Horiz. Back Porch values that I cannot simply read right off an LCD datasheet.

 

For example, I see some places, such as this NXP doc, that the Hsync Pulse Width and H Back Porch are to be considered separate and added together:

mspenard603_0-1662472141260.jpeg

However, in LCD datasheets I see Hsync Pulse Width is to be considered as fitting within the H Back Porch timing:

mspenard603_1-1662472141318.jpeg

 

0 Kudos
Reply
0 Replies