NXP Versioning Scheme for kernel/u-boot/yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Versioning Scheme for kernel/u-boot/yocto

Jump to solution
1,662 Views
mprt42
Contributor III

Hi,

quick question: How can I read the NXP versioning numbers?

e.g.: lf-5.15.71-2.2.1

How can I read that?
What does "lf" stand for?
what's 2.2.1 ?

5.15.71 is the kernel version? So it must be yocto kirkstone?

Thanks for enlightening me!

0 Kudos
Reply
1 Solution
1,628 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please refer to release note, we have some related information about these there.

The GA releases are named L<Kernel_version>_<x.y.z>.
<Kernel_version>: BSP Kernel version (For example, L5.15.71 indicates that this BSP release is based
on the kernel version 5.15.71).
<x.y.z>: Semantic versioning specification, where X is the major version, Y is the minor version, and Z is the patch version.

LF stands for Linux Factory.   IMX_LINUX_RELEASE_NOTES.pdf 

 

Regards

Harvey

View solution in original post

1 Reply
1,629 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please refer to release note, we have some related information about these there.

The GA releases are named L<Kernel_version>_<x.y.z>.
<Kernel_version>: BSP Kernel version (For example, L5.15.71 indicates that this BSP release is based
on the kernel version 5.15.71).
<x.y.z>: Semantic versioning specification, where X is the major version, Y is the minor version, and Z is the patch version.

LF stands for Linux Factory.   IMX_LINUX_RELEASE_NOTES.pdf 

 

Regards

Harvey