NXP USB lib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP USB lib

1,396 Views
Diabetoque
Contributor I

Hello,

I am a newbie in coding onto microcontrollers but i wanted to know if we can implement NXP USB lib onto a MIMXRT1176 microcontroller (on one core or both of them). Otherwise how can i implement a USB host driver on it?

Best regards,

Thx

Tags (1)
0 Kudos
Reply
1 Reply

1,380 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi!

I recommend you to check our MCUXpresso SDK, there are several USB examples including Host that can help you  with your development.

You can download appropriate SDK in this link: Welcome | MCUXpresso SDK Builder

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 Kudos
Reply